![]() |
eRPC API Reference
Rev. 1.8.1
NXP Semiconductors
|
Client side setup functions. More...
Client side setup functions.
Collaboration diagram for Client Setup:Files | |
| file | erpc_arbitrated_client_setup.h |
| file | erpc_client_setup.h |
Arbitrated client setup | |
| erpc_transport_t | erpc_arbitrated_client_init (erpc_transport_t transport, erpc_mbf_t message_buffer_factory) |
| Initializes a client that shares its transport with the server. More... | |
| void | erpc_arbitrated_client_set_error_handler (client_error_handler_t error_handler) |
| This function sets error handler function. More... | |
| void | erpc_arbitrated_client_set_crc (uint32_t crcStart) |
| Can be used to set own crcStart number. More... | |
| void | erpc_arbitrated_client_deinit (void) |
| This function de-initializes client. More... | |
Client setup | |
| void | erpc_client_init (erpc_transport_t transport, erpc_mbf_t message_buffer_factory) |
| This function initializes client. More... | |
| void | erpc_client_set_error_handler (client_error_handler_t error_handler) |
| This function sets error handler function. More... | |
| void | erpc_client_set_crc (uint32_t crcStart) |
| Can be used to set own crcStart number. More... | |
| void | erpc_client_deinit (void) |
| This function de-initializes client. More... | |
| erpc_transport_t erpc_arbitrated_client_init | ( | erpc_transport_t | transport, |
| erpc_mbf_t | message_buffer_factory | ||
| ) |
Initializes a client that shares its transport with the server.
This function initializes a client with all components necessary for sending client requests using the same transport instance as used by a server. Only one instance of the shared transport should be created. The transport arbitrator that wraps the shared transport is returned. This arbitrator, not the shared transport, should be passed to the server setup routine.
Example use:
| void erpc_arbitrated_client_set_error_handler | ( | client_error_handler_t | error_handler | ) |
This function sets error handler function.
Given error_handler function is called when error occur inside eRPC infrastructure.
| [in] | error_handler | Pointer to function error handler. |
| void erpc_arbitrated_client_set_crc | ( | uint32_t | crcStart | ) |
Can be used to set own crcStart number.
For example can be used generated crc from erpcgen which is providing when annotation is used. Accessed can be through 'extern const uint32_t erpc_generated_crc;'
| [in] | crcStart | Set start number for crc. |
| void erpc_arbitrated_client_deinit | ( | void | ) |
This function de-initializes client.
This function de-initializes client and all components which it own.
| void erpc_client_init | ( | erpc_transport_t | transport, |
| erpc_mbf_t | message_buffer_factory | ||
| ) |
This function initializes client.
| [in] | transport | Initiated transport. |
| [in] | message_buffer_factory | Initiated message buffer factory. |
This function initializes client with all components necessary for serve client request.
| void erpc_client_set_error_handler | ( | client_error_handler_t | error_handler | ) |
This function sets error handler function.
Given error_handler function is called when error occur inside eRPC infrastructure.
| [in] | error_handler | Pointer to function error handler. |
| void erpc_client_set_crc | ( | uint32_t | crcStart | ) |
Can be used to set own crcStart number.
For example can be used generated crc from erpcgen which is providing when annotation is used. Accessed can be through 'extern const uint32_t erpc_generated_crc;'
| [in] | crcStart | Set start number for crc. |
| void erpc_client_deinit | ( | void | ) |
This function de-initializes client.
This function de-initializes client and all components which it own.