![]() |
eRPC API Reference
Rev. 1.8.1
NXP Semiconductors
|
Extension setup functions. More...
Extension setup functions.
Collaboration diagram for Extension Setup:Files | |
| file | erpc_setup_extensions.h |
Typedefs | |
| typedef void * | erpc_call_timer_cb_default_t |
Functions | |
| void | erpc_init_call_progress_detection_default (erpc_call_timer_cb_default_t erpc_call_timer_cb, uint32_t waitTimeMs) |
| This function is used for initializing variables for task freeze detection. More... | |
| void | erpc_deinit_call_progress_detection_default (void) |
| This function is used for deinitialization variables for task freeze detection. | |
| bool | erpc_is_call_in_progress_default (void) |
| This function returns default eRPC call progress status. More... | |
| void | erpc_reset_in_progress_state_default (void) |
| This function resets eRPC state. More... | |
| void erpc_init_call_progress_detection_default | ( | erpc_call_timer_cb_default_t | erpc_call_timer_cb, |
| uint32_t | waitTimeMs | ||
| ) |
This function is used for initializing variables for task freeze detection.
| [in] | erpc_call_timer_cb | Callback function called when eRPC call freeze. When NULL default callback will be used. |
| [in] | waitTimeMs | Platform specific time to throw error cb in case of eRPC call freeze in [ms]. |
| bool erpc_is_call_in_progress_default | ( | void | ) |
This function returns default eRPC call progress status.
| void erpc_reset_in_progress_state_default | ( | void | ) |
This function resets eRPC state.
Can be used when user reinitialize communication between client and server.