![]() |
eRPC Generator (erpcgen)
Rev. 1.8.1
NXP Semiconductors
|
This is the complete list of members for IntegerValue, including all inherited members.
| clone() const | IntegerValue | inlinevirtual |
| getIntType() | IntegerValue | inline |
| getSize() const | IntegerValue | inlinevirtual |
| getType() const | Value | inlinevirtual |
| getTypeName() const | IntegerValue | inlinevirtual |
| getValue() const | IntegerValue | inline |
| int_type_t enum name | IntegerValue | |
| IntegerValue(int_type_t type=kSigned) | IntegerValue | inline |
| IntegerValue(uint64_t value, int_type_t type=kSigned) | IntegerValue | inline |
| IntegerValue(const IntegerValue &other) | IntegerValue | inline |
| kSigned enum value (defined in IntegerValue) | IntegerValue | |
| kSignedLong enum value (defined in IntegerValue) | IntegerValue | |
| kUnsigned enum value (defined in IntegerValue) | IntegerValue | |
| kUnsignedLong enum value (defined in IntegerValue) | IntegerValue | |
| m_intType | IntegerValue | protected |
| m_value | IntegerValue | protected |
| operator uint64_t() const | IntegerValue | inline |
| operator=(int64_t value) | IntegerValue | inline |
| toString() const | IntegerValue | inlinevirtual |
| Value(value_type_t theType) | Value | inline |
| ~Value() | Value | inlinevirtual |