![]() |
eRPC Generator (erpcgen)
Rev. 1.8.1
NXP Semiconductors
|
This is the complete list of members for OptionSpec, including all inherited members.
| Format(char *buf, unsigned optctrls) const (defined in OptionSpec) | OptionSpec | |
| isHiddenOpt(void) const (defined in OptionSpec) | OptionSpec | inline |
| isList(void) const (defined in OptionSpec) | OptionSpec | inline |
| isNoArg(void) const (defined in OptionSpec) | OptionSpec | inline |
| isNULL(void) const (defined in OptionSpec) | OptionSpec | inline |
| isSyntaxError(const char *name) const (defined in OptionSpec) | OptionSpec | |
| isValOptional(void) const (defined in OptionSpec) | OptionSpec | inline |
| isValRequired(void) const (defined in OptionSpec) | OptionSpec | inline |
| isValTaken(void) const (defined in OptionSpec) | OptionSpec | inline |
| LongOpt(void) const (defined in OptionSpec) | OptionSpec | inline |
| operator const char *() (defined in OptionSpec) | OptionSpec | inline |
| operator=(const OptionSpec &cp) (defined in OptionSpec) | OptionSpec | inline |
| operator=(const char *decl) (defined in OptionSpec) | OptionSpec | inline |
| OptChar(void) const (defined in OptionSpec) | OptionSpec | inline |
| OptionSpec(const char *decl=NULLSTR) (defined in OptionSpec) | OptionSpec | inline |
| OptionSpec(const OptionSpec &cp) (defined in OptionSpec) | OptionSpec | inline |