![]() |
eRPC Generator (erpcgen)
Rev. 1.8.1
NXP Semiconductors
|
Code generator for C. More...
#include <CGenerator.h>
Public Member Functions | |
| CGenerator (InterfaceDefinition *def) | |
| This function is constructor of CGenerator class. More... | |
| virtual | ~CGenerator () |
| This function is destructor of CGenerator class. More... | |
| virtual void | generate () |
| This function generate output code for output files. More... | |
Public Member Functions inherited from erpcgen::Generator | |
| Generator (InterfaceDefinition *def, generator_type_t generatorType) | |
| Constructor. More... | |
| virtual | ~Generator () |
| Destructor. | |
Additional Inherited Members | |
Public Types inherited from erpcgen::Generator | |
| enum | generator_type_t { kC, kPython } |
Protected Member Functions inherited from erpcgen::Generator | |
| void | openFile (std::ofstream &fileOutputStream, const std::string &fileName) |
| This function open file. More... | |
| void | generateOutputFile (const std::string &fileName, const std::string &templateName, cpptempl::data_map &templateData, const char *const kParseFile) |
| This function open file, generate output into this file and close this file. More... | |
| std::string | stripExtension (const std::string &filename) |
| StructMember * | findParamReferencedFromAnn (const StructType::member_vector_t &members, const std::string &referenceName, const std::string &annName) |
| This function will return pointer to function parameter/structure member where given reference name is referenced for. More... | |
| StructMember * | findParamReferencedFromUnion (const StructType::member_vector_t &members, const std::string &referenceName) |
| This function will return pointer to function parameter/structure member where given reference name is referenced for. More... | |
| StructMember * | findParamReferencedFrom (const StructType::member_vector_t &members, const std::string &referenceName) |
| This function will return pointer to function parameter/structure member where given reference name is referenced for. Combines findParamReferencedFromUnion and findParamReferencedFromAnn. More... | |
| std::string | getTime () |
| This function return actual time string representation. More... | |
| void | findGroupDataTypes () |
| This function finds all group's data types. | |
| cpptempl::data_list | makeGroupInterfacesTemplateData (Group *group) |
| This function sets interfaces template data. More... | |
| void | generateGroupOutputFiles (Group *group) |
| This function generates output files for defined interfaces. More... | |
| void | makeIncludesTemplateData () |
| This function sets template data for include directives from an IDL file. | |
| cpptempl::data_list | makeGroupIncludesTemplateData (Group *group) |
| This function sets template data for group include directives. More... | |
| Group * | getGroupByName (std::string name) |
| This function returns pointer to a group with specified name. More... | |
| bool | isMemberDataTypeUsingForwardDeclaration (Symbol *topSymbol, Symbol *memberSymbol) |
| This function returns information if member data type symbol is using forward declared type. More... | |
| std::string | getOutputName (Symbol *symbol, bool check=true) |
| Annotation::program_lang_t | getAnnotationLang () |
| Returns Generator flag used for annotation. More... | |
| Annotation * | findAnnotation (Symbol *symbol, std::string name) |
| Find annotation in the annotation list. More... | |
| std::vector< Annotation * > | getAnnotations (Symbol *symbol, std::string name) |
| Find annotations matching name in the annotation list. More... | |
| Value * | getAnnValue (Symbol *symbol, std::string name) |
| This function search and returns Value object for given annotation name. More... | |
| std::string | getAnnStringValue (Symbol *symbol, std::string name) |
| This function search and returns string for given annotation name. More... | |
Protected Attributes inherited from erpcgen::Generator | |
| uint16_t | m_idlCrc16 |
| cpptempl::data_map | m_templateData |
| InterfaceDefinition * | m_def |
| SymbolScope * | m_globals |
| std::vector< Group * > | m_groups |
| std::set< std::string > | reserverdWords |
| generator_type_t | m_generatorType |
| boost::filesystem::path | m_outputDirectory |
Code generator for C.
| CGenerator::CGenerator | ( | InterfaceDefinition * | def | ) |
This function is constructor of CGenerator class.
Interface definition contains all information about parsed files and builtin types.
| [in] | def | Contains all Symbols parsed from IDL files. |
|
inlinevirtual |
This function is destructor of CGenerator class.
This function close opened files.
|
virtual |
This function generate output code for output files.
This code call all necessary functions for prepare output code and parse it into output files.
Implements erpcgen::Generator.