![]() |
eRPC Generator (erpcgen)
Rev. 1.8.1
NXP Semiconductors
|
Abstract code generator base class. More...
#include <Generator.h>
Public Types | |
| enum | generator_type_t { kC, kPython } |
Public Member Functions | |
| Generator (InterfaceDefinition *def, generator_type_t generatorType) | |
| Constructor. More... | |
| virtual | ~Generator () |
| Destructor. | |
| virtual void | generate ()=0 |
| Generate output files. | |
Protected Member Functions | |
| void | openFile (std::ofstream &fileOutputStream, const std::string &fileName) |
| This function open file. More... | |
| void | generateOutputFile (const std::string &fileName, const std::string &templateName, cpptempl::data_map &templateData, const char *const kParseFile) |
| This function open file, generate output into this file and close this file. More... | |
| std::string | stripExtension (const std::string &filename) |
| StructMember * | findParamReferencedFromAnn (const StructType::member_vector_t &members, const std::string &referenceName, const std::string &annName) |
| This function will return pointer to function parameter/structure member where given reference name is referenced for. More... | |
| StructMember * | findParamReferencedFromUnion (const StructType::member_vector_t &members, const std::string &referenceName) |
| This function will return pointer to function parameter/structure member where given reference name is referenced for. More... | |
| StructMember * | findParamReferencedFrom (const StructType::member_vector_t &members, const std::string &referenceName) |
| This function will return pointer to function parameter/structure member where given reference name is referenced for. Combines findParamReferencedFromUnion and findParamReferencedFromAnn. More... | |
| std::string | getTime () |
| This function return actual time string representation. More... | |
| void | findGroupDataTypes () |
| This function finds all group's data types. | |
| virtual DataType * | findChildDataType (std::set< DataType * > &dataTypes, DataType *dataType) |
| This function finds child data types of specified data type. More... | |
| virtual void | setBinaryList (StructMember *structMember) |
| This function transform binary data type to list and set annotation to it. More... | |
| virtual cpptempl::data_map | makeGroupSymbolsTemplateData (Group *group)=0 |
| This function sets group symbols template data. More... | |
| virtual cpptempl::data_map | getFunctionTemplateData (Group *group, Function *fn)=0 |
| This function return interface function template data. More... | |
| virtual void | setTemplateComments (Symbol *symbol, cpptempl::data_map &symbolInfo)=0 |
| This function will get symbol comments and convert to language specific ones. More... | |
| cpptempl::data_list | makeGroupInterfacesTemplateData (Group *group) |
| This function sets interfaces template data. More... | |
| virtual void | generateOutputFiles (const std::string &fileNameExtension)=0 |
| This function generates output files. More... | |
| void | generateGroupOutputFiles (Group *group) |
| This function generates output files for defined interfaces. More... | |
| void | makeIncludesTemplateData () |
| This function sets template data for include directives from an IDL file. | |
| cpptempl::data_list | makeGroupIncludesTemplateData (Group *group) |
| This function sets template data for group include directives. More... | |
| Group * | getGroupByName (std::string name) |
| This function returns pointer to a group with specified name. More... | |
| bool | isMemberDataTypeUsingForwardDeclaration (Symbol *topSymbol, Symbol *memberSymbol) |
| This function returns information if member data type symbol is using forward declared type. More... | |
Protected Attributes | |
| uint16_t | m_idlCrc16 |
| cpptempl::data_map | m_templateData |
| InterfaceDefinition * | m_def |
| SymbolScope * | m_globals |
| std::vector< Group * > | m_groups |
| std::set< std::string > | reserverdWords |
| generator_type_t | m_generatorType |
| boost::filesystem::path | m_outputDirectory |
is used. | |||||||
This function returns symbol output name. Can be different to getName() when
| |||||||
| std::string | getOutputName (Symbol *symbol, bool check=true) | ||||||
| Annotation::program_lang_t | getAnnotationLang () | ||||||
| Returns Generator flag used for annotation. More... | |||||||
| Annotation * | findAnnotation (Symbol *symbol, std::string name) | ||||||
| Find annotation in the annotation list. More... | |||||||
| std::vector< Annotation * > | getAnnotations (Symbol *symbol, std::string name) | ||||||
| Find annotations matching name in the annotation list. More... | |||||||
| Value * | getAnnValue (Symbol *symbol, std::string name) | ||||||
| This function search and returns Value object for given annotation name. More... | |||||||
| std::string | getAnnStringValue (Symbol *symbol, std::string name) | ||||||
| This function search and returns string for given annotation name. More... | |||||||
Abstract code generator base class.
| Generator::Generator | ( | InterfaceDefinition * | def, |
| generator_type_t | generatorType | ||
| ) |
Constructor.
Interface definition contains all information about parsed files and builtin types.
| [in] | def | Contains all Symbols parsed from IDL files. |
|
protected |
Find annotation in the annotation list.
| [in] | symbol | Symbol from which is annotation extracted. |
| [in] | name | Annotation name. |
|
protectedvirtual |
This function finds child data types of specified data type.
This function should be overridden by language specific generator, if there is a need to transform data types.
| [in,out] | dataTypes | Vector of found data types. |
| [in] | dataType | Top data type. |
|
protected |
This function will return pointer to function parameter/structure member where given reference name is referenced for. Combines findParamReferencedFromUnion and findParamReferencedFromAnn.
| [in] | members | Members contain references members and searched members. |
| [in] | referenceName | Name of reference for which is member searched. |
|
protected |
This function will return pointer to function parameter/structure member where given reference name is referenced for.
| [in] | members | Members contain references members and searched members. |
| [in] | referenceName | Name of reference for which is member searched. |
| [in] | annName | Annotation name for which is member searched. |
|
protected |
This function will return pointer to function parameter/structure member where given reference name is referenced for.
| [in] | members | Members contain references members and searched members. |
| [in] | referenceName | Name of reference for which is member searched. |
|
protected |
This function generates output files for defined interfaces.
| [in] | group | Pointer to a group. |
|
protected |
This function open file, generate output into this file and close this file.
| [in] | fileName | Output file name. |
| [in] | templateName | Name of template file, which is used for parser. |
| [in] | templateData | Template data used for parser. |
| [in] | kParseFile | Templates strings converted from text file by txt_to_c.py used for parser. |
| TemplateException | Thrown, when parse template data into output is not successfully. |
|
protectedpure virtual |
This function generates output files.
This function call functions for generating client/server header/source files.
| [in] | fileNameExtension | Extension for file name (for example for case that each interface will be generated in its set of output files). |
Implemented in erpcgen::PythonGenerator.
|
protected |
|
protected |
Find annotations matching name in the annotation list.
| [in] | symbol | Symbol from which is annotation extracted. |
| [in] | name | Annotation name. |
|
protected |
This function search and returns string for given annotation name.
| [in] | symbol | Symbol from which is annotation extracted. |
| [in] | name | Given annotation name. |
|
protectedpure virtual |
This function return interface function template data.
This function return interface function template data with all data, which are necessary for generating output code for output files.
| [in] | group | Pointer to a group. |
| [in] | fn | From this are set interface function template data. |
| [in] | fnIndex | Function index. |
Implemented in erpcgen::PythonGenerator.
|
protected |
This function returns pointer to a group with specified name.
| [in] | name | Name of the searched group. |
|
protected |
This function return actual time string representation.
|
protected |
This function returns information if member data type symbol is using forward declared type.
| [in] | topSymbol | Symbol data type which is using as a member memberSymbol data type. |
| [in] | memberSymbol | Member symbol data type of topSymbol. |
| True | when memberSymbol is using forward declared type. |
| False | when memberSymbol is not using forward declared type. |
|
protected |
This function sets template data for group include directives.
| [in] | group | Pointer to a group. |
|
protected |
This function sets interfaces template data.
This function sets interfaces template data with all data, which are necessary for generating output code for output files.
| [in] | group | Pointer to a group. |
|
protectedpure virtual |
This function sets group symbols template data.
This function sets group symbols template data with all data, which are necessary for generating output code for output files.
| [in] | group | Pointer to a group. |
Implemented in erpcgen::PythonGenerator.
|
protected |
This function open file.
| [in] | fileName | Output file name. |
| [in,out] | fileOutputStream | Opened output file stream. |
| std::runtime_error | Thrown, when can't create directory. |
| std::runtime_error | Thrown, when file is not open. |
|
inlineprotectedvirtual |
This function transform binary data type to list and set annotation to it.
| [in] | structMember | Structure member, Function parameter or Union member. |
|
protectedpure virtual |
This function will get symbol comments and convert to language specific ones.
| [in] | symbol | Pointer to symbol. |
| [in,out] | symbolInfo | Data map, which contains information about symbol. |
Implemented in erpcgen::PythonGenerator.
|
protected |
| [in] | filename |
|
protected |
Interface definitions.
|
protected |
Type of generator.
|
protected |
Symbol scope data.
|
protected |
List of groups.
|
protected |
Storing crc16 of IDL files and erpcgen version.
|
protected |
Output file path.
|
protected |
Data prepared for templates files.
|
protected |
Program language reserved words.