![]() |
eRPC Generator (erpcgen)
Rev. 1.8.1
NXP Semiconductors
|
Structure data type. More...
#include <StructType.h>
Public Types | |
| typedef std::vector< StructMember * > | member_vector_t |
Public Types inherited from erpcgen::DataType | |
| enum | _data_type { kAliasType, kArrayType, kBuiltinType, kEnumType, kFunctionType, kListType, kStructType, kUnionType, kVoidType } |
| Supported data types. | |
Public Types inherited from erpcgen::Symbol | |
| enum | symbol_type_t { kConstSymbol, kEnumMemberSymbol, kFunctionSymbol, kInterfaceSymbol, kProgramSymbol, kStructMemberSymbol, kTypenameSymbol, kUnionCaseMemberSymbol, kAliasTypeSymbol, kArrayTypeSymbol, kBuiltinTypeSymbol, kEnumTypeSymbol, kFunctionTypeSymbol, kListTypeSymbol, kStructTypeSymbol, kUnionTypeSymbol } |
| Supported symbol types. | |
Public Member Functions | |
| StructType (const std::string &name) | |
| Constructor. More... | |
| StructType (const Token &tok) | |
| Constructor. More... | |
| void | addMember (StructMember *newMember) |
| This function will add struct member to the struct. More... | |
| SymbolScope & | getScope () |
| This function returns symbol scope. More... | |
| member_vector_t & | getMembers () |
| This function returns struct members vector. More... | |
| virtual bool | isStruct () const |
| This function return "true" value for identify struct type. More... | |
| virtual std::string | getDescription () const |
| This function returns description about the struct. More... | |
| bool | containListMember () |
| This function return true, when has member, which contains list type. More... | |
| bool | containStringMember () |
| This function return true, when has member, which contains string type. More... | |
| bool | containByrefMember () |
| This function return true, when has member, which contains flag byref. More... | |
Public Member Functions inherited from erpcgen::DataType | |
| DataType (_data_type dataType) | |
| Constructor. More... | |
| DataType (const std::string &name, _data_type dataType) | |
| Constructor. More... | |
| DataType (const std::string &name, _data_type dataType, symbol_type_t symbolType) | |
| Constructor. More... | |
| DataType (const Token &tok, _data_type dataType, symbol_type_t symbolType) | |
| Constructor. More... | |
| _data_type | getDataType () const |
| This function returns data type. More... | |
| DataType * | getTrueDataType () |
| This function returns pointer to true data type instead of alias. More... | |
| DataType * | getTrueContainerDataType () |
| This function returns pointer to true data type (enum, builtin, structs) except lists and arrays. More... | |
| virtual bool | isAlias () const |
| This function return "false" value as default for identify alias type. More... | |
| virtual bool | isArray () const |
| This function return "false" value as default for identify array type. More... | |
| virtual bool | isBinary () const |
| This function return "false" value as default for identify binary type. More... | |
| virtual bool | isBool () const |
| This function return "false" value as default for identify bool type. More... | |
| virtual bool | isBuiltin () const |
| This function return "false" value as default for identify builtin type. More... | |
| virtual bool | isEnum () const |
| This function return "false" value as default for identify enum type. More... | |
| virtual bool | isFunction () const |
| This function return "false" value as default for identify function type. More... | |
| virtual bool | isList () const |
| This function return "false" value as default for identify list type. More... | |
| virtual bool | isScalar () const |
| This function return "false" value as default for identify scalar builtin type. More... | |
| virtual bool | isString () const |
| This function return "false" value as default for identify string type. More... | |
| virtual bool | isUString () const |
| This function return "false" value as default for identify ustring type. More... | |
| virtual bool | isUnion () const |
| This function return "false" value as default for identify union type. More... | |
| virtual bool | isVoid () const |
| This function return "false" value as default for identify void type. More... | |
Public Member Functions inherited from erpcgen::Symbol | |
| Symbol (symbol_type_t symType) | |
| Constructor. More... | |
| Symbol (symbol_type_t symType, const std::string &name) | |
| Constructor. More... | |
| Symbol (symbol_type_t symType, const Token &tok) | |
| Constructor. More... | |
| virtual | ~Symbol () |
| Destructor. | |
| symbol_type_t | getSymbolType () const |
| This function returns symbol type. More... | |
| const std::string & | getName () const |
| This function returns symbol name. More... | |
| void | setName (const std::string &newName) |
| This function set symbol name. More... | |
| token_loc_t & | getLocation () |
| This function returns location for symbol. More... | |
| void | setLocation (const token_loc_t &loc) |
| This function set location for symbol. More... | |
| int | getFirstLine () const |
| This function return first line from location of symbol. More... | |
| int | getLastLine () const |
| This function return last line from location of symbol. More... | |
| void | addAnnotation (const Annotation &a) |
| This function add annotation to vector of symbol annotations. More... | |
| std::string | printAnnotations () |
| This function returns description about annotation. More... | |
| Annotation * | findAnnotation (std::string name, Annotation::program_lang_t lang) |
| Find annotation in the annotation list. More... | |
| std::vector< Annotation * > | getAnnotations (std::string name, Annotation::program_lang_t lang) |
| Find annotations matching name in the annotation list. More... | |
| const std::vector< Annotation > & | getAnnotations () const |
| Return all Symbol annotations. More... | |
| Value * | getAnnValue (const std::string annName, Annotation::program_lang_t lang) |
| This function search and returns Value object for given annotation name. More... | |
| std::string | getAnnStringValue (const std::string annName, Annotation::program_lang_t lang) |
| This function search and returns string for given annotation name. More... | |
| std::string | getMlComment () |
| This function returns multiline comment for this symbol declared in IDL file. More... | |
| void | setMlComment (std::string comment) |
| This function set multiline comment for this symbol declared in IDL file. More... | |
| std::string | getIlComment () |
| This function returns inline comment for this symbol declared in IDL file. More... | |
| void | setIlComment (std::string comment) |
| This function set inline comment for this symbol declared in IDL file. More... | |
Protected Attributes | |
| SymbolScope | m_scope |
| member_vector_t | m_members |
Protected Attributes inherited from erpcgen::DataType | |
| _data_type | m_dataType |
Protected Attributes inherited from erpcgen::Symbol | |
| symbol_type_t | m_symbolType |
| std::string | m_name |
| token_loc_t | m_location |
| std::vector< Annotation > | m_annotations |
| std::string | m_mlComment |
| std::string | m_ilComment |
Structure data type.
| typedef std::vector<StructMember *> erpcgen::StructType::member_vector_t |
Vector of Struct members.
|
inline |
Constructor.
This function set name to given name.
| [in] | name | Given name. |
|
inline |
Constructor.
This function set symbol token to given token.
| [in] | tok | Given token. |
| void StructType::addMember | ( | StructMember * | newMember | ) |
This function will add struct member to the struct.
The function will add struct member given by pointer newMember to the struct members vector m_members. Also this member will be added as symbol to struct symbol scope m_scope.
| [in] | newMember | Struct member pointer, which is added to struct members vector. |
| bool StructType::containByrefMember | ( | ) |
This function return true, when has member, which contains flag byref.
| bool StructType::containListMember | ( | ) |
This function return true, when has member, which contains list type.
| bool StructType::containStringMember | ( | ) |
This function return true, when has member, which contains string type.
|
virtual |
This function returns description about the struct.
Reimplemented from erpcgen::Symbol.
|
inline |
This function returns struct members vector.
|
inline |
This function returns symbol scope.
|
inlinevirtual |
This function return "true" value for identify struct type.
| true | Always return true. |
Reimplemented from erpcgen::DataType.
|
protected |
Vector of structure members.
|
protected |
Symbol scope of current structure.