![]() |
eRPC Generator (erpcgen)
Rev. 1.8.1
NXP Semiconductors
|
Discriminated union data type. More...
#include <UnionType.h>
Public Types | |
| typedef std::vector< UnionCase * > | case_vector_t |
Public Types inherited from erpcgen::DataType | |
| enum | _data_type { kAliasType, kArrayType, kBuiltinType, kEnumType, kFunctionType, kListType, kStructType, kUnionType, kVoidType } |
| Supported data types. | |
Public Types inherited from erpcgen::Symbol | |
| enum | symbol_type_t { kConstSymbol, kEnumMemberSymbol, kFunctionSymbol, kInterfaceSymbol, kProgramSymbol, kStructMemberSymbol, kTypenameSymbol, kUnionCaseMemberSymbol, kAliasTypeSymbol, kArrayTypeSymbol, kBuiltinTypeSymbol, kEnumTypeSymbol, kFunctionTypeSymbol, kListTypeSymbol, kStructTypeSymbol, kUnionTypeSymbol } |
| Supported symbol types. | |
Public Member Functions | |
| UnionType (const std::string &name, const std::string &discriminatorName) | |
| Constructor. More... | |
| UnionType (const Token &tok, const std::string &discriminatorName) | |
| Constructor. More... | |
| StructType * | getParentStruct () |
| Returns the struct owning this union. | |
| void | setParentStruct (StructType *parent) |
| Sets the struct owning this union. | |
| void | addCase (UnionCase *unionCase) |
| This function will add union case to current union. More... | |
| virtual std::string | getDescription () const |
| This function returns description about the union. More... | |
| virtual bool | isUnion () const |
| This function return "true" value for identify union type. More... | |
| bool | isNonEncapsulatedUnion () const |
| This function return "true" value for identify non-encapsulated discriminated union type. More... | |
| case_vector_t & | getCases () |
| This function returns union cases vector. More... | |
| case_vector_t | getUniqueCases () |
| This function returns unique union cases vector. More... | |
| bool | addUnionMemberDeclaration (const std::string &name, DataType *dataType) |
| This function adds unique union member declaration. More... | |
| StructType & | getUnionMembers () |
| This function returns struct of union members. More... | |
| StructMember * | getUnionMemberDeclaration (const std::string &name) |
| This function returns union member declaration. More... | |
| std::string | getDiscriminatorName () |
| This function returns union discriminator name. More... | |
| void | printUnionMembers () |
| This function prints information about union members. | |
| bool | declarationExists (const std::string &name) |
| This function is looking for member declaration. More... | |
Public Member Functions inherited from erpcgen::DataType | |
| DataType (_data_type dataType) | |
| Constructor. More... | |
| DataType (const std::string &name, _data_type dataType) | |
| Constructor. More... | |
| DataType (const std::string &name, _data_type dataType, symbol_type_t symbolType) | |
| Constructor. More... | |
| DataType (const Token &tok, _data_type dataType, symbol_type_t symbolType) | |
| Constructor. More... | |
| _data_type | getDataType () const |
| This function returns data type. More... | |
| DataType * | getTrueDataType () |
| This function returns pointer to true data type instead of alias. More... | |
| DataType * | getTrueContainerDataType () |
| This function returns pointer to true data type (enum, builtin, structs) except lists and arrays. More... | |
| virtual bool | isAlias () const |
| This function return "false" value as default for identify alias type. More... | |
| virtual bool | isArray () const |
| This function return "false" value as default for identify array type. More... | |
| virtual bool | isBinary () const |
| This function return "false" value as default for identify binary type. More... | |
| virtual bool | isBool () const |
| This function return "false" value as default for identify bool type. More... | |
| virtual bool | isBuiltin () const |
| This function return "false" value as default for identify builtin type. More... | |
| virtual bool | isEnum () const |
| This function return "false" value as default for identify enum type. More... | |
| virtual bool | isFunction () const |
| This function return "false" value as default for identify function type. More... | |
| virtual bool | isList () const |
| This function return "false" value as default for identify list type. More... | |
| virtual bool | isScalar () const |
| This function return "false" value as default for identify scalar builtin type. More... | |
| virtual bool | isString () const |
| This function return "false" value as default for identify string type. More... | |
| virtual bool | isUString () const |
| This function return "false" value as default for identify ustring type. More... | |
| virtual bool | isStruct () const |
| This function return "false" value as default for identify struct type. More... | |
| virtual bool | isVoid () const |
| This function return "false" value as default for identify void type. More... | |
Public Member Functions inherited from erpcgen::Symbol | |
| Symbol (symbol_type_t symType) | |
| Constructor. More... | |
| Symbol (symbol_type_t symType, const std::string &name) | |
| Constructor. More... | |
| Symbol (symbol_type_t symType, const Token &tok) | |
| Constructor. More... | |
| virtual | ~Symbol () |
| Destructor. | |
| symbol_type_t | getSymbolType () const |
| This function returns symbol type. More... | |
| const std::string & | getName () const |
| This function returns symbol name. More... | |
| void | setName (const std::string &newName) |
| This function set symbol name. More... | |
| token_loc_t & | getLocation () |
| This function returns location for symbol. More... | |
| void | setLocation (const token_loc_t &loc) |
| This function set location for symbol. More... | |
| int | getFirstLine () const |
| This function return first line from location of symbol. More... | |
| int | getLastLine () const |
| This function return last line from location of symbol. More... | |
| void | addAnnotation (const Annotation &a) |
| This function add annotation to vector of symbol annotations. More... | |
| std::string | printAnnotations () |
| This function returns description about annotation. More... | |
| Annotation * | findAnnotation (std::string name, Annotation::program_lang_t lang) |
| Find annotation in the annotation list. More... | |
| std::vector< Annotation * > | getAnnotations (std::string name, Annotation::program_lang_t lang) |
| Find annotations matching name in the annotation list. More... | |
| const std::vector< Annotation > & | getAnnotations () const |
| Return all Symbol annotations. More... | |
| Value * | getAnnValue (const std::string annName, Annotation::program_lang_t lang) |
| This function search and returns Value object for given annotation name. More... | |
| std::string | getAnnStringValue (const std::string annName, Annotation::program_lang_t lang) |
| This function search and returns string for given annotation name. More... | |
| std::string | getMlComment () |
| This function returns multiline comment for this symbol declared in IDL file. More... | |
| void | setMlComment (std::string comment) |
| This function set multiline comment for this symbol declared in IDL file. More... | |
| std::string | getIlComment () |
| This function returns inline comment for this symbol declared in IDL file. More... | |
| void | setIlComment (std::string comment) |
| This function set inline comment for this symbol declared in IDL file. More... | |
Additional Inherited Members | |
Protected Attributes inherited from erpcgen::DataType | |
| _data_type | m_dataType |
Protected Attributes inherited from erpcgen::Symbol | |
| symbol_type_t | m_symbolType |
| std::string | m_name |
| token_loc_t | m_location |
| std::vector< Annotation > | m_annotations |
| std::string | m_mlComment |
| std::string | m_ilComment |
Discriminated union data type.
| typedef std::vector<UnionCase *> erpcgen::UnionType::case_vector_t |
Vector of Union cases.
|
inline |
Constructor.
This function set data type to union data type and name to given name. It will also set discriminator name.
| [in] | name | Given name. |
| [in] | discriminatorName | Discriminator name. |
|
inline |
Constructor.
This function set data type to union data type and symbol token to given token. It will also set discriminator name.
| [in] | tok | Given token.. |
| [in] | discriminatorName | Discriminator name. |
| void UnionType::addCase | ( | UnionCase * | unionCase | ) |
This function will add union case to current union.
| [in] | unionCase | Given union case. |
| bool UnionType::addUnionMemberDeclaration | ( | const std::string & | name, |
| DataType * | dataType | ||
| ) |
This function adds unique union member declaration.
| [in] | name | Union case name. |
| [in] | dataType | Union case data type. |
| bool UnionType::declarationExists | ( | const std::string & | name | ) |
This function is looking for member declaration.
| [in] | name | Name of union member. |
| true | when declaration already exist. |
| false | when declaration don't exist. |
|
inline |
This function returns union cases vector.
|
virtual |
This function returns description about the union.
Reimplemented from erpcgen::Symbol.
|
inline |
This function returns union discriminator name.
| StructMember * UnionType::getUnionMemberDeclaration | ( | const std::string & | name | ) |
This function returns union member declaration.
| [in] | name | Name of union member. |
|
inline |
This function returns struct of union members.
| UnionType::case_vector_t UnionType::getUniqueCases | ( | ) |
This function returns unique union cases vector.
|
inline |
This function return "true" value for identify non-encapsulated discriminated union type.
| true | True when m_discriminator is not set. |
|
inlinevirtual |
This function return "true" value for identify union type.
| true | Always return true. |
Reimplemented from erpcgen::DataType.