Overview
========
The sai_edma_transfer example shows how to use sai driver with EDMA:

In this example, one sai instance playbacks the audio data stored in flash/SRAM using EDMA channel.

Toolchain supported
===================
- IAR embedded Workbench  9.32.1
- Keil MDK  5.37
- MCUXpresso  11.7.0
- GCC ARM Embedded  10.3.1

Hardware requirements
=====================
- Mini/micro USB cable
- MIMXRT1170-EVKB board
- Personal Computer
- Headphone(OMTP standard)

Board settings
==============
Ensure the resistors mounted below:
R2001,R2002,R2003,R2004,R2005,R2006 and R2007.

Measurement
J97: BCLK
J98: SYNC
J101-1: R
J101-4: L
J101-5: GND

Prepare the Demo
================
1.  Connect a USB cable between the host PC and the OpenSDA USB port on the target board. 
2.  Open a serial terminal with the following settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board.
4. Insert the headphones into the headphone jack on MIMXRT1170-EVKB board (J101).
5. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo
================
note:This demo uses codec master mode(internal pll mode).

When the demo runs successfully, you can hear the tone and the log would be seen on the OpenSDA terminal like:

~~~~~~~~~~~~~~~~~~~
SAI example started!
SAI EDMA example finished!
~~~~~~~~~~~~~~~~~~~