This .zip file contains the source code and binary used by the application note AN3763

AXE debugging tools:
- header and library for the AXE debugging tool

AXE post linker:
- Win32 postlinker for the AXE scheduler tasks' .elf files

AXE scheduler files:
- binary files for the AXE scheduler
- header files needed to program tasks for the AXE scheduler

AXE scheduler task setup files:
- linker command file for the AXE scheduler tasks
- start the assembler code for the AXE scheduler tasks

PPC additional files:
- additional files to create an e300 application for the AXE scheduler

PPC-AXE driver:
- PPC-AXE driver library 
- PPC-AXE driver header files

type conversion library:
- library for the type conversion between floating point and fixed point
- header file