This is release 1.0 of the ENG_POS API and example files.
The user should refer to Application Note AN3769 "Using the Engine Position 
eTPU Function" which is available from Freescale.

_____________________________________________________________________________

Files included in this package:
===============================
    eng_pos\readme.txt                 Rev: see below  - This file.
    eng_pos\etpu_app_eng_pos.c         Rev : 1.6 - The C code file for the ENG_POS API.
    eng_pos\etpu_app_eng_pos.h         Rev : 1.6 - The header file for the ENG_POS API.
    eng_pos\eng_pos_example.c          Rev : 1.4 - Example C code file for MPC5633M  device.
    eng_pos\eng_pos_example.h          Rev : 1.2 - Example header file for MPC5633M  device.
    eng_pos\eng_pos_etpu_gct_example.c Rev : 1.2 - Example C code file generated by GCT.
    eng_pos\eng_pos_etpu_gct_example.h Rev : 1.1 - Example header file generated by GCT.
    eng_pos\MPC563M_intram.dld         Rev : 1.1 - Linker file.
    eng_pos\makefile                   Rev : 1.4 - A GNU makefile used to build the example
                                                   code.

NB The example referred to above is a very simple example which uses the tooth 
generation function to provide an input stimulus to the engine position functions.
This is a an example provided in addition to the more complex example referred to 
in AN3769 "Using the Engine Position (CRANK and CAM) eTPU Functions".
In order to use this simple example short eTPU_A0 to eTPU_A1 and short 
eTPU_A14 to eTPU_A15. This connects the tooth generator outputs to the engine
position inputs. This example produces no output. It simply generates a TCR2 (angle clock).


The following files are needed in order to compile and use the example code:
_____________________________________________________________________________

  From AN3768SW "eTPU Automotive Set (Set 2)"
    etpu_set2\etpu_set2.h          - Image of eTPU set2 function code.
_____________________________________________________________________________

  From AN3801SW "Using the Tooth Generator eTPU Function"
    tooth_gen\etpu_toothgen.c - C code file for tooth generator function.
    tooth_gen\etpu_toothgen.h - header file for tooth generator function.
_____________________________________________________________________________     

  From AN2864SW "General C Functions for the eTPU."
    utils\etpu_util.c   - C code file for utility functions.
    utils\etpu_util.h   - header file for utility functions.
    utils\etpu_struc.h  - Register and bit field definitions for the eTPU.
_____________________________________________________________________________     

  From AN2855SW "Using GPIO on MPC5500"
    mpc5500\fs_gpio.c - MPC5500 GPIO low level driver C code file.
    mpc5500\fs_gpio.h - MPC5500 GPIO low level driver header file.
    mpc5500\crt0.s    - Start-up file
_____________________________________________________________________________     

	Available from Freescale
    mpc5500\mpc563m.h  - Register and bit field definitions for MPC5633M.
    mpc5500\typedefs.h - Defines all for data types.
____________________________________________________________________________     

All of the above files are available from the Freescale website.
_____________________________________________________________________________

Readme.txt HISTORY
------------------
  $Log: readme.txt,v $
  Revision 1.15  2009/02/03 15:03:26  r47354
  *** empty log message ***

  Revision 1.14  2009/02/02 15:13:56  r47354
  *** empty log message ***

  Revision 1.13  2009/02/02 11:01:37  r47354
  *** empty log message ***

  Revision 1.12  2009/02/02 10:59:16  r47354
  *** empty log message ***

  Revision 1.11  2009/01/08 15:57:31  r47354
  *** empty log message ***

  Revision 1.10  2009/01/08 12:08:49  r47354
  *** empty log message ***

  Revision 1.9  2008/11/26 15:34:22  r47354
  *** empty log message ***

  Revision 1.8  2008/11/13 10:56:49  r47354
  *** empty log message ***

  Revision 1.7  2008/11/13 10:51:44  r47354
  *** empty log message ***

  Revision 1.6  2008/11/13 10:50:41  r47354
  *** empty log message ***

  Revision 1.5  2008/09/25 14:36:48  r47354
  *** empty log message ***

  Revision 1.4  2008/09/25 14:32:10  r47354
  *** empty log message ***

  Revision 1.3  2008/06/23 14:26:50  r47354
  *** empty log message ***

  Revision 1.2  2008/06/06 12:02:48  r47354
  *** empty log message ***