#####################################################################
# This file contains the key numbering scheme per CSE documetation. #
# and also the associated key number.                               #
# This key number will be written to a header file                  #
# so it can be used by core code as input to the CSE                #
# CMAC command.                                                     #
#                                                                   #
# In this file lines beginning with a '#' are comments.             #
# Blank lines will be ignored by the script.                        #
# The fields are spaced delimited.                                  #
# One key name key number pair per line.                            #
#####################################################################
CSE_SECRET_KEY     0
CSE_MASTER_ECU_KEY 1
CSE_BOOT_MAC_KEY   2
CSE_BOOT_MAC       3
CSE_KEY_1          4
CSE_KEY_2          5
CSE_KEY_3          6
CSE_KEY_4          7
CSE_KEY_5          8
CSE_KEY_6          9
CSE_KEY_7          10
CSE_KEY_8          11
CSE_KEY_9          12
CSE_KEY_10         13 
CSE_RAM_KEY        14