#################################################################
# This file contains the keys to be used for CMAC calculations. #
# and also the associated key number.                           #
# This key number will be written to a header file              #
# so it can be used by core code as input to the CSE            #
# CMAC command.                                                 #
#                                                               #
# In this file lines beginning with a '#' are comments.         #
# Blank lines will be ignored by the script.                    #
# The fields are spaced delimited.                              #
# One key number, key pair per line.                            #
#################################################################

CSE_KEY_10 68B674CB8198A2503A285100F4DDC40A

CSE_KEY_7 2b7e151628aed2a6abf7158809cf4f3c