##############################################################
# This file contains the sections to be processed            #
# and also the key number which is to be used                #
# in the CMAC generation.                                    #
# This key number will be written to a header file           #
# so it can be used by core code as input to the CSE         #
# CMAC command.                                              #
#                                                            #
# In this file lines beginning with a '#' are comments.      #
# Blank lines will be ignored by the script.                 #
# The fields are spaced delimited.                           #
# One section, key number pair per line.                     #
##############################################################

CMAC_APP_CODE1 CSE_KEY_7
CMAC_APP_CODE2 CSE_KEY_7
CMAC_APP_CODE3 CSE_KEY_10