=============================================================================
List of generated methods in project: ProcessorExpert

THIS TEXT DESCRIPTION IS GENERATED BY THE TOOL. DO NOT MODIFY IT.
=============================================================================

Module "FTM2"      (component Init_FTM_HCS08)
   - FTM2_Init -This method initializes registers of the FTM module according to the Peripheral Initialization settings. Call 
                this method in user code to initialize the module. By default, the method is called by PE automatically; see 
                "Call Init method" property of the component for more details.

Module "FTM0"      (component Init_FTM_HCS08)
   - FTM0_Init -This method initializes registers of the FTM module according to the Peripheral Initialization settings. Call 
                this method in user code to initialize the module. By default, the method is called by PE automatically; see 
                "Call Init method" property of the component for more details.

Module "MTIM1"     (component Init_MTIM_HCS08)
   - MTIM1_Init -This method initializes registers of the MTIM module according to this Peripheral Initialization settings. 
                Call this method in user code to initialize the module. By default, the method is called by PE automatically; 
                see "Call Init method" property of the component for more details.

Module "PortH"     (component Init_GPIO_VAR2)
   - PortH_Init -This method initializes registers of the GPIO module according to the Peripheral Initialization settings. Call 
                this method in user code to initialize the module. By default, the method is called by PE automatically; see 
                "Call Init method" property of the component for more details.

Module "SCI"       (component Init_SCI_HCS08)
   - SCI_Init -This method initializes registers of the SCI module according to this Peripheral Initialization settings. Call 
                this method in user code to initialize the module. By default, the method is called by PE automatically; see 
                "Call Init method" property of the component for more details.

Module "SPI"       (component Init_SPI_HCS08)
   - SPI_Init -This method initializes registers of the SPI module according to this Peripheral Initialization settings. Call 
                this method in user code to initialize the module. By default, the method is called by PE automatically; see 
                "Call Init method" property of the component for more details. 

Module "GPIO1"     (component Init_GPIO_VAR2)
   - GPIO1_Init -This method initializes registers of the GPIO module according to the Peripheral Initialization settings. Call 
                this method in user code to initialize the module. By default, the method is called by PE automatically; see 
                "Call Init method" property of the component for more details.

Module "ADC"       (component Init_ADC_HCS08)
   - ADC_Init -This method initializes registers of the ADC module according to this Peripheral Initialization settings. Call 
                this method in user code to initialize the module. By default, the method is called by PE automatically; see 
                "Call Init method" property of the component for more details.

Module "GPIO2"     (component Init_GPIO_VAR2)
   - GPIO2_Init -This method initializes registers of the GPIO module according to the Peripheral Initialization settings. Call 
                this method in user code to initialize the module. By default, the method is called by PE automatically; see 
                "Call Init method" property of the component for more details.

Module "GPIO3"     (component Init_GPIO_VAR2)
   - GPIO3_Init -This method initializes registers of the GPIO module according to the Peripheral Initialization settings. Call 
                this method in user code to initialize the module. By default, the method is called by PE automatically; see 
                "Call Init method" property of the component for more details.

Module "Cpu"       (component MC9S08PT60_64)
   - Cpu_EnableInt -Enables maskable interrupts
   - Cpu_DisableInt -Disables maskable interrupts

===================================================================================