/**
@page EEPROM_Emulation_demo_readme   Platinum
@verbatim
******************** (C) COPYRIGHT 2013 Freescale ******************************
* File Name          : Readme.txt
* Author             : Freescale
* Date First Issued  : 06/25/2013 : Version 1.0.0
* Description        : Description of the template example.
********************************************************************************
* History:
* 06/25/2013 : Version 1.0.0
********************************************************************************
* THE PRESENT SOFTWARE WHICH IS FOR GUIDANCE ONLY AIMS AT PROVIDING CUSTOMERS
* WITH CODING INFORMATION REGARDING THEIR PRODUCTS IN ORDER FOR THEM TO SAVE TIME.
* AS A RESULT, FREESCALE SHALL NOT BE HELD LIABLE FOR ANY DIRECT,
* INDIRECT OR CONSEQUENTIAL DAMAGES WITH RESPECT TO ANY CLAIMS ARISING FROM THE
* CONTENT OF SUCH SOFTWARE AND/OR THE USE MADE BY CUSTOMERS OF THE CODING
* INFORMATION CONTAINED HEREIN IN CONNECTION WITH THEIR PRODUCTS.
********************************************************************************
@endverbatim

@par Example description
     ===================
This example provides a template for the sample code. It demonstrates how to 
configure RTC with 1Hz and  how to switch clock mode from FEE to FEI as well as
how to initialize UART. 
It will echo the character entered in the terminal and at meanwhile 
it will flash red led at every 1s.

@par Code configuration
     ===================
Make sure the following macros are defined in ke06_config.h: \n
   USE_FEE and  \n
   EXT_CLK_FREQ_KHZ macro is defined to 10000.


@par Directory contents
     ===================
- platforms/ke06_config.h     library and board Configuration file
- projects/ke06/isr.h         Interrupt handler installation
- projects/ke06/EEPROM_Emulation_demo.c    Main program


@par Hardware environment
     ====================
 - Board: freedom FRDM-KE06Z, revA
  
@par How to use it
     =============
In order to make the program work, you must do the following :
- Rebuild all project files and load demo code into the device
- Connect J6 USB port to the computer that will find serial terminal port
- Open the serial terminal
- Configure the serial terminal to protocol: 8-N-1, 115200bps, and flow control: none
- Run the example
- Type any character which will echo to the terminal window


@verbatim
************************END OF FILE********************************************
@endverbatim

*/