![]() |
#include <etpu_crank_emul.h>
Definition at line 86 of file etpu_crank_emul.h.
Data Fields | |
| uint8_t | teeth_per_sync |
| uint24_t | blank_time |
| uint8_t | blank_teeth |
| ufract24_t | gap_ratio |
| ufract24_t | win_ratio_normal |
| ufract24_t | win_ratio_across_gap |
| ufract24_t | win_ratio_after_gap |
| ufract24_t | win_ratio_after_timeout |
| uint24_t | first_tooth_timeout |
|
|
A number of teeth ignored after initialization. Definition at line 95 of file etpu_crank_emul.h. Referenced by fs_etpu_crank_config(), and fs_etpu_crank_init(). |
|
|
A TCR1 time period after initialization during which teeth are ignored. Definition at line 93 of file etpu_crank_emul.h. Referenced by fs_etpu_crank_config(), and fs_etpu_crank_init(). |
|
|
A TCR1 time period after the first tooth (after blank_teeth) when a timeout will be deemed to have happened. Definition at line 110 of file etpu_crank_emul.h. Referenced by fs_etpu_crank_config(), and fs_etpu_crank_init(). |
|
|
A fraction used to perform the ABA gap test. For a crank wheel with a gap: gap_ratio * tooth_period_B > tooth_period_A. For a crank wheel with an additional tooth: gap_ratio * tooth_period_A > tooth_period_B. Definition at line 97 of file etpu_crank_emul.h. Referenced by fs_etpu_crank_config(), and fs_etpu_crank_init(). |
|
|
A number of teeth (including the missing teeth in gap) corresponding to a segment which is needed for the Cam to log enough Cam transitions so that it enables to recognize the correct engine half-cycle and achieve synchronozation. It must be a multiple of (teeth_till_gap + teeth_in_gap). Definition at line 88 of file etpu_crank_emul.h. Referenced by fs_etpu_crank_config(), and fs_etpu_crank_init(). |
|
|
A fraction used to derive the acceptance window for the first tooth after the gap. Definition at line 104 of file etpu_crank_emul.h. Referenced by fs_etpu_crank_config(), and fs_etpu_crank_init(). |
|
|
A fraction used to derive the acceptance window for the second tooth after the gap. Definition at line 106 of file etpu_crank_emul.h. Referenced by fs_etpu_crank_config(), and fs_etpu_crank_init(). |
|
|
A fraction used to derive the acceptance window for the tooth following a timeout condition. Definition at line 108 of file etpu_crank_emul.h. Referenced by fs_etpu_crank_config(), and fs_etpu_crank_init(). |
|
|
A fraction used to derive the acceptance window for the next normal tooth. Definition at line 102 of file etpu_crank_emul.h. Referenced by fs_etpu_crank_config(), and fs_etpu_crank_init(). |
Generated by ![]() |
© Freescale Semiconductor Inc. 2004 - 2012. All Rights Reserved. |