![]() |
#include <etpu_crank_emul.h>
Definition at line 35 of file etpu_crank_emul.h.
Data Fields | |
| const uint8_t | chan_num |
| const uint8_t | priority |
| const uint8_t | polarity |
| const uint8_t | teeth_till_gap |
| const uint8_t | teeth_in_gap |
| const uint8_t | teeth_per_cycle |
| const uint24_t | tcr2_ticks_per_tooth |
| const uint8_t | log_tooth_periods |
| const uint32_t | link_cam |
| const uint32_t | link_1 |
| const uint32_t | link_2 |
| const uint32_t | link_3 |
| const uint32_t | link_4 |
| uint32_t * | cpba |
| uint32_t * | cpba_tooth_period_log |
|
|
Channel number of the CRANK channel. Definition at line 37 of file etpu_crank_emul.h. Referenced by fs_etpu_crank_init(), fs_etpu_crank_set_speed(), and fs_etpu_crank_set_sync(). |
|
|
Channel parameter base address. Set cpba = 0 to use automatic allocation of eTPU DATA RAM for CRANK channel parameters using the eTPU utility function fs_etpu_malloc (recommanded), or assign the cpba manually by an address where the CRANK channel parameter space will start from, e.g. 0xC3FC8100. Definition at line 70 of file etpu_crank_emul.h. Referenced by fs_etpu_crank_config(), fs_etpu_crank_get_states(), fs_etpu_crank_init(), fs_etpu_crank_set_speed(), and fs_etpu_crank_set_sync(). |
|
|
Base address of the CRANK tooth period log buffer in eTPU DATA RAM. Set cpba_tooth_period_log = 0 to use automatic allocation of eTPU DATA RAM for this buffer using the eTPU utility function fs_etpu_malloc (recommanded), or assign the p_tooth_period_log manually by an address where the CRANK buffer will start. The memory does not need to be allocated if FS_ETPU_CRANK_FM1_TOOTH_PERIODS_LOG_OFF is set. Definition at line 75 of file etpu_crank_emul.h. Referenced by fs_etpu_crank_copy_tooth_period_log(), and fs_etpu_crank_init(). |
|
|
The first set of 4 link numbers to send when stall conditions accure. Definition at line 62 of file etpu_crank_emul.h. Referenced by fs_etpu_crank_init(). |
|
|
The second set of 4 link numbers to send when stall conditions accure. Definition at line 64 of file etpu_crank_emul.h. Referenced by fs_etpu_crank_init(). |
|
|
The third set of 4 link numbers to send when stall conditions accure. Definition at line 66 of file etpu_crank_emul.h. Referenced by fs_etpu_crank_init(). |
|
|
The fourth set of 4 link numbers to send when stall conditions accure. Definition at line 68 of file etpu_crank_emul.h. Referenced by fs_etpu_crank_init(). |
|
|
Set of 4 link numbers to send to reset the Cam log. Up to 4 Cam channel numbers can be used. In case of a single Cam on channel 1, use 0x01010101. Definition at line 59 of file etpu_crank_emul.h. Referenced by fs_etpu_crank_init(). |
|
|
An option to record tooth_periods. It can be one of:
Definition at line 55 of file etpu_crank_emul.h. Referenced by fs_etpu_crank_init(). |
|
|
CRANK transition polarity. It defines which type of transitions are captured. It can be one of:
Definition at line 39 of file etpu_crank_emul.h. Referenced by fs_etpu_crank_init(). |
|
|
Channel priority for the CRANK channel. Definition at line 38 of file etpu_crank_emul.h. Referenced by fs_etpu_crank_init(). |
|
|
A number of TCR2 angle ticks per one tooth. It can be any value between 1 and 1024. Definition at line 53 of file etpu_crank_emul.h. Referenced by fs_etpu_crank_init(). |
|
|
A number of missing teeth in one gap. This can be assigned a value of 1, 2, 3 (for eTPU and eTPU2), up to 7 (for eTPU2+), or 0. The value 0 indicates there is an additional tooth instead of missing teeth. Definition at line 46 of file etpu_crank_emul.h. Referenced by fs_etpu_crank_init(). |
|
|
A number of teeth (including missing teeth in gap) per an engine cycle (720 degrees). It must be a multiple of (teeth_till_gap + teeth_in_gap). Definition at line 50 of file etpu_crank_emul.h. Referenced by fs_etpu_crank_copy_tooth_period_log(), and fs_etpu_crank_init(). |
|
|
A number of physical teeth between 2 gaps. This is the number of physical teeth on the crank wheel divided by the number of (equally spaced) gaps on the wheel. Definition at line 43 of file etpu_crank_emul.h. Referenced by fs_etpu_crank_init(). |
Generated by ![]() |
© Freescale Semiconductor Inc. 2004 - 2012. All Rights Reserved. |