![]() |
#include <etpu_spark.h>
Definition at line 62 of file etpu_spark.h.
Data Fields | |
| int24_t | angle_offset_recalc |
| uint24_t | dwell_time_min |
| uint24_t | dwell_time_max |
| uint24_t | multi_on_time |
| uint24_t | multi_off_time |
| uint8_t | spark_count |
| single_spark_config_t * | p_single_spark_config |
| uint8_t | generation_disable |
|
|
The recalculation offset angle as a number of TCR2 ticks. At the end of one spark the start angle of the next spark is calculated according to the actual engine speed and end_angle. The calculation is repeated once again in order to adjust to a speed change at a defined angular position before the originaly calculated start_angle. This position is given by angle_offset_recalc. Definition at line 64 of file etpu_spark.h. Referenced by fs_etpu_spark_config(), and fs_etpu_spark_init(). |
|
|
The maximum spark dwell time as a number of TCR1 ticks. Definition at line 73 of file etpu_spark.h. Referenced by fs_etpu_spark_config(), and fs_etpu_spark_init(). |
|
|
The minimum spark dwell time as a number of TCR1 ticks. Definition at line 71 of file etpu_spark.h. Referenced by fs_etpu_spark_config(), and fs_etpu_spark_init(). |
|
|
This parameter disables/enables the generation of output pulses. It can be assigned one of the values: Definition at line 82 of file etpu_spark.h. Referenced by fs_etpu_spark_config(), and fs_etpu_spark_init(). |
|
|
The multi-pulse OFF-time as a number of TCR1 ticks. Definition at line 77 of file etpu_spark.h. Referenced by fs_etpu_spark_config(), and fs_etpu_spark_init(). |
|
|
The multi-pulse ON-time as a number of TCR1 ticks. Definition at line 75 of file etpu_spark.h. Referenced by fs_etpu_spark_config(), and fs_etpu_spark_init(). |
|
|
Pointer to the first item of an array of the single spark configuration structures. Definition at line 80 of file etpu_spark.h. Referenced by fs_etpu_spark_config(), and fs_etpu_spark_init(). |
|
|
The count of single sparks per engine-cycle. Definition at line 79 of file etpu_spark.h. Referenced by fs_etpu_spark_config(), and fs_etpu_spark_init(). |
Generated by ![]() |
© Freescale Semiconductor Inc. 2004 - 2012. All Rights Reserved. |