![]() |
Definition in file etpu_tg.c.
#include "etpu_tg.h"
#include "etpu_util.h"
Go to the source code of this file.
Functions | |
| uint32_t | fs_etpu_tg_init (struct tg_instance_t *p_tg_instance, struct tg_config_t *p_tg_config) |
| This function initializes eTPU channels to run TG function. | |
| uint32_t | fs_etpu_tg_config (struct tg_instance_t *p_tg_instance, struct tg_config_t *p_tg_config) |
| This function changes the TG configuration. | |
| uint32_t | fs_etpu_tg_get_states (struct tg_instance_t *p_tg_instance, struct tg_states_t *p_tg_states) |
| This function reads state parameter values of the TG function. | |
Variables | |
| uint32_t | fs_etpu_data_ram_start |
| uint32_t | fs_etpu_data_ram_ext |
|
||||||||||||
|
This function changes the TG configuration.
Definition at line 193 of file etpu_tg.c. References tg_config_t::accel_ratio, tg_instance_t::cpba, FS_ETPU_TG_OFFSET_ACCEL_RATIO, FS_ETPU_TG_OFFSET_GENERATION_DISABLE, FS_ETPU_TG_OFFSET_TOOTH_PERIOD_TARGET, tg_config_t::generation_disable, and tg_config_t::tooth_period_target. |
|
||||||||||||
|
This function reads state parameter values of the TG function.
Definition at line 231 of file etpu_tg.c. References tg_instance_t::cpba, FS_ETPU_TG_OFFSET_TOOTH_COUNTER_CYCLE, FS_ETPU_TG_OFFSET_TOOTH_PERIOD_ACTUAL, tg_states_t::tooth_counter_cycle, and tg_states_t::tooth_period_actual. |
|
||||||||||||
|
|
|
|
|
Referenced by fs_etpu_tg_init(). |
Generated by ![]() |
© Freescale Semiconductor Inc. 2004 - 2012. All Rights Reserved. |