![]() |
#include <etpu_fuel.h>
Definition at line 104 of file etpu_fuel.h.
Data Fields | |
| uint8_t | error |
| uint24_t | injection_time_applied |
| int24_t | injection_start_angle |
|
|
This is the error status of FUEL. It may include the following error flags:
Definition at line 106 of file etpu_fuel.h. Referenced by fs_etpu_fuel_get_states(). |
|
|
This is the last injection tdc_angle-relative start angle as a number of TCR2 ticks. Definition at line 115 of file etpu_fuel.h. Referenced by fs_etpu_fuel_get_states(). |
|
|
This is the applied injection time of the last injection. The value corresponds to commanded injection_time, but it may slightly differ in case of rapid acceleration or late call of fs_etpu_fuel_update_injection_time(). Definition at line 111 of file etpu_fuel.h. Referenced by fs_etpu_fuel_get_states(). |
Generated by ![]() |
© Freescale Semiconductor Inc. 2004 - 2012. All Rights Reserved. |