![]() |
#include <etpu_knock.h>
Definition at line 38 of file etpu_knock.h.
Data Fields | |
| const uint8_t | chan_num |
| const uint8_t | priority |
| const uint8_t | polarity |
| const uint24_t | tdc_angle |
| uint32_t * | cpba |
| uint32_t * | cpba_windows |
|
|
Channel number of the KNOCK channel. Definition at line 40 of file etpu_knock.h. Referenced by fs_etpu_knock_config(), and fs_etpu_knock_init(). |
|
|
Channel parameter base address. Set cpba = 0 to use automatic allocation of eTPU DATA RAM for KNOCK channel parameters using the eTPU utility function fs_etpu_malloc (recommanded), or assign the cpba manually by an address where the KNOCK channel parameter space will start from, e.g. 0xC3FC8100. Definition at line 48 of file etpu_knock.h. Referenced by fs_etpu_knock_config(), and fs_etpu_knock_init(). |
|
|
Base address of the knock windows array in eTPU DATA RAM. Set cpba_windows = 0 to use automatic allocation of the eTPU DATA RAM space corresponding to the window_count value, using the eTPU utility function fs_etpu_malloc (recommanded), or assign the cpba_windows manually by an address, e.g. 0xC3FC8100. Definition at line 53 of file etpu_knock.h. Referenced by fs_etpu_knock_config(), and fs_etpu_knock_init(). |
|
|
KNOCK polarity. It can one any of:
Definition at line 42 of file etpu_knock.h. Referenced by fs_etpu_knock_init(). |
|
|
Channel priority for the KNOCK channel. Definition at line 41 of file etpu_knock.h. Referenced by fs_etpu_knock_init(). |
|
|
The cylinder Top Dead Center as a number of TCR2 angle ticks relative to zero engine angle, in a range corresponding to 0-720 degrees. Definition at line 45 of file etpu_knock.h. Referenced by fs_etpu_knock_init(). |
Generated by ![]() |
© Freescale Semiconductor Inc. 2004 - 2012. All Rights Reserved. |