Release Name: MCUXpresso Software Development Kit (SDK)
Release Version: 2.6.0
Package License: LA_OPT_NXP_Software_License.htm - Production Use, Section 2.3 applies

KSDK_Peripheral_Driver     Description: Peripheral drivers are designed for  
                           the most common use cases identified for the      
                           underlying hardware block.                        
                           Author: Freescale                                 
                           Version: 2.x.x                                    
                           License: Open Source - BSD-3-Clause               
                           Format: source code                               
                           name: KSDK Peripheral Driver                      
                           Location: devices/<device>/drivers                

usb                        version: 2.2.0                                    
                           Location: middleware/usb                          
                           Description: Freescale USB stack. This is a       
                           version of the USB stack that has been integrated 
                           with the MCUXpresso SDK.                          
                           License: Open Source - BSD-3-Clause               
                           Author: Freescale                                 
                           name: USB                                         
                           Format: source code                               

fatfs                      Approved Open Source License: Yes                 
                           Author: Electronic Lives Mfg. by ChaN of Ageo     
                           city, Japan (hobbyist)                            
                           Description: FatFs is a generic FAT file system   
                           module for small embedded systems.                
                           Format: source code                               
                           License: Open Source - FatFs License,             
                           middleware/fatfs/LICENSE.txt                      
                           Location: middleware/fatfs                        
                           name: FatFs                                       
                           URL: http://elm-chan.org/fsw/ff/00index_e.html    
                           version: 0.13b                                    

cmsiscore                  Author: ARM                                       
                           parentversion: 5.1.1                              
                           URL:                                              
                           https://github.com/ARM-software/CMSIS_5/releases/t
                           ag/5.3.0                                          
                           name: CMSIS Core header files                     
                           Format: source code                               
                           License: Apache License 2.0, See CMSIS/LICENSE.txt
                           Location: CMSIS/Include                           
                           version: 5.1.1 (CMSIS Download 5.3.0)             
                           Description: Industry-standard header files       
                           distributes by ARM for cortex-M cores             

cmsis_drivers              Author: Freescale                                 
                           version: 2.x.x                                    
                           Format: source code                               
                           Description: CMSIS Peripheral drivers are designed
                           to provide hardware independent APIs which make   
                           application reusable across a wide range of       
                           supported microcontroller devices.                
                           name: KSDK CMSIS Peripheral Drivers               
                           Location: devices/<device>/cmsis_drivers          
                           License: Open Source - Apache 2.0 & BSD-3-Clause