Overview
========
The Simple PWM Interrupt project is to demonstrate usage of the SDK CTimer driver as a PWM with interrupt callback functions
In this example an IO pin connected to the LED is used as a PWM output line to generate a PWM signal.
With an interrupt callback the PWM duty cycle is changed frequently in such a way that the LED brightness can be varied.

Toolchain supported
===================
- IAR embedded Workbench  8.50.1
- Keil MDK  5.29
- GCC ARM Embedded  8.3.1
- MCUXpresso  11.1.0

Hardware requirements
=====================
- Mini/micro USB cable
- LPCXpresso55S16 board
- Personal Computer

Board settings
==============
The jumper setting:
    Default jumpers configuration does not work,  you will need to add JP20 and JP21 (JP22 optional for ADC use)

Prepare the Demo
================
1.  Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J1) on the board
2.  Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board.
4.  Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo
================
The log below shows example output of the CTimer simple PWM demo using interrupts in the terminal window:
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
CTimer example to generate a PWM signal
This example uses interrupts to update the PWM duty cycle
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

The red led will adjust brightness automatic.
Customization options
=====================