Overview
========
The CWT Example project is a demonstration program that uses the KSDK software to set up secure counter and instruction timer.
Then tests several times the expected value with value in secure counter. After that miscompare fault is intentionally generated
by comparing secure counter with wrong value. At the end application let the instruction timer reach zero and generate another timeout fault.


Toolchain supported
===================
- IAR embedded Workbench  8.50.1
- Keil MDK  5.29
- GCC ARM Embedded  8.3.1
- MCUXpresso  11.1.0

Hardware requirements
=====================
- Mini/micro USB cable
- LPCXpresso55S16 board
- Personal Computer

Board settings
==============
The jumper setting:
    Default jumpers configuration does not work,  you will need to add JP20 and JP21 (JP22 optional for ADC use)

Prepare the Demo
================
1.  Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J1) on the board
2.  Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board.
4.  Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo
================
When the demo runs successfully, the terminal displays similar information like the following:
~~~~~~~~~~~~~~~~~~

CWT Peripheral Driver Example

CWT IRQ Reached
* Miscompare fault occured *

intruction timer:   fffc5
intruction timer:   c615e
intruction timer:   8c34e
intruction timer:   5251a
intruction timer:   18703
CWT IRQ Reached
* Timeout fault occured *

End of example

Note:
To keep the program running correctly, it is recommended to perform a power on reset (POR; SW2) after loading the application.
SW reset does not clear pending fault flags.
Customization options
=====================