Overview
========
The SCTimer 16-bit counter project is a demonstration program of the SDK SCTimer driver operation when using the SCTimer counter
as two 16-bit counters.
The example toggles an output per counter when a match occurs.

Toolchain supported
===================
- IAR embedded Workbench  8.50.1
- Keil MDK  5.29
- GCC ARM Embedded  8.3.1
- MCUXpresso  11.1.0

Hardware requirements
=====================
- Micro USB cable
- LPCXpresso55S16 board
- Personal Computer

# Board settings

```
Output signal		Board location
SCT0_OUT2    		J12-12
SCT0_OUT6    		J12-14
```

The jumper setting:
    Default jumpers configuration does not work,  you will need to add JP20 and JP21 (JP22 optional for ADC use)

# Prepare the Demo

1.  Connect a micro USB cable between the host PC and the LPC-Link USB port (J1) on the target board.
2.  Open a serial terminal with the following settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board.
4.  Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Board settings
==============

Prepare the Demo
================

Running the demo
================
The log below shows example output in the terminal window:
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
SCTimer example to use it in 16-bit mode
The example shows both 16-bit counters running and toggling an output periodically
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

You'll see PWM signals on J12_12 and J12_14 using an oscilloscope
Customization options
=====================