Overview
========
The spi_interrupt example shows how to use spi functional API to do interrupt transfer:

In this example, one spi instance as master and another spi instance as slave. Master sends a piece of data to slave,
and check if the data slave received is correct.

Toolchain supported
===================
- IAR embedded Workbench  8.50.1
- Keil MDK  5.29
- GCC ARM Embedded  8.3.1
- MCUXpresso  11.1.0

Hardware requirements
=====================
- Micro USB cable
- LPCXpresso55S16 board
- Personal Computer

Board settings
==============
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
    Master_board(SPI7)           Slave_board(SPI2)                          
Pin Name   Board Location     Pin Name   Board Location                     
MISO       J9    pin 11       MISO       J12   pin 5
MOSI       J9    pin 9        MOSI       J12   pin 9
SCK        J9    pin 13       SCK        J12   pin 7
SSEL1      J9    pin 2        SSEL0      J12   pin 13
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

The jumper setting:
    Default jumpers configuration does not work,  you will need to add JP20 and JP21 (JP22 optional for ADC use)
    
Prepare the Demo
================
1.  Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J1) on the board
2.  Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board.
4.  Reset the SoC and run the project.

Running the demo
================
When the demo runs successfully, the log would be seen on the CMSIS DAP terminal like:

~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
SPI one board interrupt example started!

SPI transfer finished!
​~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
Customization options
=====================