RELEASE: LPC4300CMSIS_20120417
1/ Added IAR port of BOOTFAST example (high-speed mode from SPIFI or external Flash)
2/ New version of SPIFI library supports large SPIFI >= 256 Mb and does not use memset/memcpy

RELEASE CMSIS for REV A 20120331
01/. Updated legalese on source, header and abstract files
02/. Separated SDIO driver into SDIF and SDMMC components
03/. Updated correct setting for Deep Sleep: replace the value in line "#define PWR_SLEEP_MODE_DEEP_SLEEP 0x3F00AA" with 0x3000AA
04/. Updated CGU Set PLL0 function
05/. Updated GPIO driver for external interrupt
06/. Added Gpio_Input example to configure GPIO to read the state of a particular pin
07/. Added Gpio_ExtInt example to use GPIO as source of an external interrupt
08/. Added OTP_API example
09/. Updated LPC18xx.h: Corrected the define for the number of priority bits (must be 3 and not 4)
10/. Fixed minor bugs in I2S driver
11/. Updated makesection and makefile to compile and run GNU projects on Linux:
	- Use / instead of \ in folder paths.
	- Move TOOL_PATH definition to "makeconfig" file.
	- Correct the EXDIR path in USB_Hid makefile
12/. Updated to run on the new board (Hitex LPC1850EVA-A4):
	- Updated the new .FLM file for Keil projects
	- I2S: example can play sound in a loop
	- ATIMER, Cortex-M3, EMC, GPDMA, GPIO, NVIC, UART, SSP: using USART0 instead of UART1, update abstract files and comments
	- EMAC: updated the correct configuration for ACD pin (PF.9 - ADC1 channel 2) and all Ethernet pins; use USART0 instead of UART1
	- SCT: using RGB led output signals, updated .fzm file, added red state diagram
	- GPIO_LedBlinky example: change RGB LED color every second
13/. Updated .chm file and Examples Description.
14/. RTC: fixed bugs in:
	- lpc18xx_rtc.c: RTC_CntIncrIntConfig(), RTC_AlarmIntConfig(): checking disble bit
	- Rtc_Alarm: EVRT_IRQHandler() clear event pending before serving RTC interrupt routine
	
RELEASE CMSIS for REV A 20120131
1./ Updated IAR projects: added SPIFI targets
2./ Fix format issue in SD card reader example(USBDEV_ROM/MassStorage)
3./ Updated copyright header for source, header and abstract files

RELEASE CMSIS for REV A 20111230
1/ added LCD Term.h, lpc18xx_aes_otp.h, lpc18xx_sdio driver, lpc_sdmmc.h, AES_test example, CGU_measureFreq example, I2C_TouchLEDs example, sdio_readwrite SPIFI_ReadWrite example
2/ Updated CGU driver to support setting flexible output freq for PLL0 USB and Audio
3/ Updated CAN driver to support 2 independent CANs
4/ Updated GPDMA, GPIO, PWR, LCD, I2S, scu drivers for buid issues
5/ Updated ATIMER_WIC example to use new EVENT Router IRQ macro
6/ Updated all Keil init files to use fixed load address
7/ Updated USB_cdc, massStorage, all usb Rom examples

RELEASE CMSIS for REV A 20111209
1/ New LPC18xx.h header file. Changes GPIO structure.
2/ Addition of lpc18xx_emc.c and lpc18xx_emc.h to configure memory on Hitex board.
3/ Addition of spifi_rom_api.h, spifi_drv_M3.lib and SPIFI_ROM_support.doc SPIFI driver package
4/ Updated SPIFI programming driver for Keil MDK which uses the SPIFI lib
5/ New BOOTFAST example shows how to boot from external flash or QSPI and ramp to 180 MHz

RELEASE CMSIS for REV A 20111130
1./ lpc18xx_lcd.h LCD_CFG_type add member pcd, lpc18xx_lcd.c add init pcd in LCD_Init function
2./ protect MAX and MIN macro in lpc_types.h
3./ Add getPC function to ARM,GNU, IAR startup_lpc18xx.s
4./ Add VTOR init in SystemInit function
5./ Change All ADC examples to use ADC port 0
6./ These example: CortexM3_Mpu, Pwr_DeepPowerDown, Timer_FreqMeasure, SCT_SimpleMatch and all USBDEV_ROM examples Keil project was adjusted
7./ SDRAM example and LCD example was changed not to use uint64_t in NS2CLK function
8./ Nvic_VectorTableRelocation.c
removed: 
#if __RAM_MODE__//Run in RAM mode
  memcpy((void *)VTOR_OFFSET, (const void *)0x10000000, 256*4);
#else
  memcpy((void *)VTOR_OFFSET, (const void *)0x1C000000, 256*4);
#endif

added:
memcpy((void *)VTOR_OFFSET, (const void *)(getPC()& 0xFF000000), 256*4);
9./ Pwr_PowerDown change method for testing this feature


RELEASE CMSIS for REV A 20111028
1./ Add GNU support
2./ Addition of new Keil flash drivers for eFlash and SPIFI
3./ Change of Keil projects to support eFlash and SPIFI operation

PRE-RELEASE CMSIS for REV A 20111011
1/ PowerDown Example IAR issue fixed
2/ Upgraded CMSIS to version 2.10
3/ Upgraded Core header to Rev A
4/ lpc18xx_can.h remove all bitrates from 8Mhz, add bitrates from 12Mhz
	/** Bitrate: 100K */
	#define CAN_BITRATE100K12MHZ           0x00004509
	/** Bitrate: 125K */
	#define CAN_BITRATE125K12MHZ           0x00004507
	/** Bitrate: 250K */
	#define CAN_BITRATE250K12MHZ           0x00004503
	/** Bitrate: 500K */
	#define CAN_BITRATE500K12MHZ            0x00004501
	/** Bitrate: 1000K */
	#define CAN_BITRATE1000K12MHZ          0x00004500
5./ lpc18xx_cgu.* add PLL audio clock, modify alloc connect table and CGU_Entity_ControlReg_Offset
6./ lpc18xx_evrt.h
	add EVRT_SRC_SDIO
7./ lpc18xx_i2s.h separate LPC_I2S0 and LPC_I2S1
8./ lpc18xx_scu.h
	redefine, add pin modes and add pin functions 4->7
9./ debug_frmwrk.c
	changed pin mode for UART RXD0 and UART RXD1
10./ lpc_can.c replace LPC_CAN by LPC_CAN0
11./ lpc18xx_i2c.* replace i2c pin configurations
12./ lpc18xx_ssp.c down default clock speed to 100kHz
13./ Examples\CCAN\CCan_SimpleTxRx\CCan_SimpleTxRx.c change RD pin mode to enable input buffer
14./ Examples\EMAC\Emac_EasyWeb\emac.c
		replace MII and RMII pin setting by source from CodeBundle
15./ Examples\EMC\Emc_Sdram\SDRAM_Init.c and Examples\EMC\Emc_NorFlash\SST39VF320.c
		replace EMC pin setting to be compatible with Rev A
16./ Examples\I2S\I2s_Audio\I2s_Audio.c
		replace I2S pin setting to be compatible with Rev A
		replace I2S to I2S0
17./ Examples\LCD\Lcd_Demo\IS42S16400D.c
		replace EMC pin setting to be compatible with Rev A
18./ Examples\SSP\All SSP examples: replace SSP pin setting to be compatible with Rev A
19./ Timer_Capture and Timer_FreqMeasure: replace Capture input pin setting to be compatible with Rev A
20./ Examples\UART\All UART examples: replace UART pin setting to be compatible with Rev A
21./ Examples\USBDEV\USB_*\usbhw.c
		replace USB pin setting to be compatible with Rev A
		correct clock in Init function

RELEASE: LPC1800CMSIS_20110829
1./ Add GNU Support
modify pasting in can.c to be compatible with GCC

RELEASE: LPC1800CMSIS_20110729
1./ IAR flash support is moved to Tools folder
2./ ADC.h fixed macro ADC_CR_BITACC
3./ I2S.h fixed comment
	from #endif /* LPC17XX_SSP_H_ */
	to #endif /* LPC18XX_I2S_H_ */
4./ ADC.c fix ADC_Init Clock by rounding clk div value
5./ i2s.c fixed some comment
6./ EMC Nor Flash renamed file  flash programing function
7./ SDRAM can run at MAX EMC Speed
8./ Removed flash programing support for LHF00L28

RELEASE: LPC1800CMSIS_20110627
1./ Fix abstract
2./ Fix I2S FreqConfig mistake
3./ Add DFU Driver and App


RELEASE: LPC1800CMSIS_20110613
1./ Add DSP Document
2./ Speed Up External FLash Mode
3./ Add IAR Flash Support
4./ Fix GPDMA Flash transfer issue in IAR
5./ Set default taget is EXFLASH(Keil only)

************************************************************************************************************************************************
RELEASE: LPC1800CMSIS_20110603
1./ Add DSP_lib into Core folder
2./ Update core_cmFunc.h and core_cmInstr.h for solving conflict with IAR EWARM version 6.20 or later
3./ add IAR startup file and IAR support files in Core\DeviceSupport\NXP\LPC18xx
4./ Modify SystemInit function to support RAM mode
	#if (__RAM_MODE__)
    	SCB->VTOR = 0x10000000;
	#endif
5./ Modify CCU1 and CCU2 struct in LPC18xx.h
6./ Fix bug in uart_set_divisors function
7./ Change UART clock source from XTAL to PLL1 in uart driver
8./ Fix RTC bugs
9./ Modify lpc18xx_GPDMA.c to support IAR compiler
10./ Modify lpc18xx_cgu.c to support IAR compiler
11./ Update lpc_types.h to support IAR compiler
12./ Fix bugs in I2S driver
13./ Remove Warnings
14./ Change new header, add more comments
15./ Standalize example, project, output names
16./ Support IAR EWARM (RAM mode)
17./ SUpport Hitex Board as default
18./ Modify hardware configuration in abstract files
19./ Set default Target to RAM mode

************************************************************************************************************************************************
RELEASE: LPC1800CMSIS_20110514
1./ Change all Keil example projects from device Cortex M3 to LPC1850
2./ change all examples to support Hitex board only
3./ Verify all project option
4./ separated CGU and PWR into 2 independent drivers

************************************************************************************************************************************************
RELEASE: LPC1800CMSIS_20110421
1./ Add CAN driver:
	Drivers/include/lpc18xx_can.h
	Drivers/source/lpc18xx_can.c

2./ Add CAN example for simple Transceiver
	Examples\C_CAN\simpleTxRx

3./ Add 4 USB Rom examples:
	USB_DFU
	USB_HID
	USB_MassStorage
	USB_Composite

4./ Enable _printf function
	debug_frmwrk.h:
		uncomment _printf function declaration
	debug_frmwrk.c:
		uncomment _printf function

************************************************************************************************************************************************
RELEASE: LPC1800CMSIS_20110401

1./ Change all Keil example proiects from device NXP LPC1768 to ARM Cortex-M3

2./ Fix bug in I2C driver (customer feedback)
	Problem description: 
		I2C_MasterTransferData() is not able to 
		(1) Send, 
		(2) doing a repeated Start and 
		(3) starting to receive with one function call. 
		Problem is that the repeated start is not generated, but a retransmission of the 
		last word is startet. 
	Solve: change 
		I2Cx->I2CONCLR = I2C_I2CONCLR_SIC; 
		I2Cx->I2CONSET = I2C_I2CONSET_STA; 
	to 
		I2Cx->I2CONSET = I2C_I2CONSET_STA; 
		I2Cx->I2CONCLR = I2C_I2CONCLR_SIC; 
		in function I2C_Start ()

3./ lpc18xx_timer.c:
	Function TIM_ClearIntPending():
		Change TIMx->IR |= TIM_IR_CLR(IntFlag);
		To     TIMx->IR = TIM_IR_CLR(IntFlag);
	Function TIM_ClearIntCapturePending():
		Change TIMx->IR |= (1<<(4+IntFlag));
		To     TIMx->IR = (1<<(4+IntFlag));
	Function TIM_GetCaptureValue(): 
		Add return 0;

4./ EMC - Nor Flash: remove example build target for FLASH mode as it only can run in RAM mode.

5./ SCT: update Fizzim tool to version 1.1

6./ Tools:
	Update Flash burning for LHF00L28 and SST39X320X

************************************************************************************************************************************************

RELEASE: LPC1800CMSIS_20110324

1./ Current support hardwares:
	- NXP LPC1800 Evaluation board through definition 'BOARD_NXP_EA'
	- Hitex LPC1800 Board through definition 'BOARD_HITEX_LPC1800'
    Some examples can run on LPC1800 Evaluation board, some can run on Hitex board...Please refer to abstract.txt

2./ Addin new flash support under Tools/Flash/SST39X320X

3./ lpc18xx_evrt.c:
	Change EVRTx->SET_EN |= (1<<(uint8_t)EVRT_Src);
	To     EVRTx->SET_EN = (1<<(uint8_t)EVRT_Src);
	Purpose: prevent clearing other set bits as writing '0' has no effect

4./ Fix ATIMER_WIC example:
	- Configure 32KHZ osc in lpc18xx_atimer.c
	- Call the configuration function in atimer_wic.c

5./ Fix RTC_Alarm example:
	- Configure 32KHZ osc in lpc18xx_rtc.c
	- Update Rtc_Alarm.c

6./ Add in PWR_PowerDown example

7./ Add in PWR_DeepPowerDown example

8./ All example in PWR are modified to wait for '1' sent from PC's COM port to start

9./ Fix LCD Logic4.3 example to run on Hitex LPC1800 Board

10./ Add in GPDMA Flash_2_Ram_Test example

11./ EMC EXT_SDRAM example: join IS42S16400D.c and MT48LC4M32B2.c into SDRAM_Init.c

12./ lpc18xx_i2s.c: update I2S_FreqConfig() function

************************************************************************************************************************************************

RELEASE: LPC1800CMSIS_20110311

1./ This package is compliant to CMSIS 2.0

2./ Add in 'Tools' folder which contains neccessary material for building project, examples like flash burning,..

3./ Examples are given in Keil uVision 4 project

4./ Current support hardwares:
	- NXP LPC1800 Evaluation board through definition 'BOARD_NXP_EA'

5./ Examples can run:
	- RAM (debug) mode
	- ROM (Flash, stand alone) mode
		+ External Nor Flash. Flash Part supporting:
			1) LHF00L28

6./ Each example folder has an 'abstract.txt' file, this is where user can start

7./ Below is list of drivers and examples:
	- ADC (lpc18xx_adc):
		+ ADC_Interrupt
		+ ADC_Polling
		+ ADC_Burst
		+ ADC_Dma
	- ATIMER (lpc18xx_atimer):
		+ ATIMER_interrupt
	- PWR (lpc18xx_clkpwr):
		+ CLKPWR_Sleep
		+ CLKPWR_DeepSleep
	- DAC (lpc18xx_dac):
		+ DAC_WaveGenerator
		+ DAC_Dma
	- EMAC (lpc18xx_emac):
		+ EMAC_EasyWeb
	- EMC (no driver):
		+ EXT_SDRAM
		+ NOR_FLASH
	- GPDMA (lpc18xx_gpdma):
		+ GPDMA_Ram2Ram
		+ GPDMA_LinkList
	- GPIO (lpc18xx_gpio):
		+ GPIO_LedBlinky
	- I2C (lpc18xx_i2c):
		+ I2C_Master
	- I2S (lpc18xx_i2s):
		+ I2S_Audio
	- LCD (lpc18xx_lcd)
	- MCPWM (lpc18xx_mcpwm):
		+ MCPWM_Simple
	- SCU (lpc18xx_scu)
	- QEI (lpc18xx_qei):
		+ QEI_Velo
	- RIT (lpc18xx_rit):
		+ RIT_Interrupt
	- RTC (lpc18xx_rtc):
		+ RTC_Calib
		+ RTC_Alarm
	- SSP (lpc18xx_ssp):
		+ SSP_SPI
		+ SSP_Microwire
		+ SSP_TI
	- TIMER (lpc18xx_timer):
		+ TIMER_Capture
		+ TIMER_MatchInterrupt
		+ TIMER_FreqMeasure
	- UART (lpc18xx_uart):
		+ UART_Autobaud
		+ UART_Dma
		+ UART_Interrupt
		+ UART_Polling
		+ UART_RS485
	- SCT(LPC18xx_SCT):
		+ SCT_Capture
		+ SCT_Match
	- WWDT (lpc18xx_wwdt):
		+ WWDT_Interrupt
	- CORTEXM3 (no driver):
		+ CORTEXM3_BitBanding
		+ CORTEXM3_MPU
		+ CORTEXM3_PriviledgeMode
	- USBDEV (no driver):
		+ USBDEV_VirtualCOM
		+ USBDEV_MassStorage
	- NVIC (no driver):
		+ NVIC_Priority
		+ NVIC_VecRelocation
	- EVRT (lpc18xx_evrt)