CMSIS : Cortex Microcontroller Software Interface Standard
==========================================================

Introduction
~~~~~~~~~~~~
CMSIS defines for a Cortex-M Microcontroller System:

    * A common way to access peripheral registers and a 
      common way to define exception vectors.
    * The register names of the Core Peripherals and the 
      names of the Core Exception Vectors.
    * An device independent interface for RTOS Kernels 
      including a debug channel.

By using CMSIS compliant software components, the user can 
easier re-use template code. CMSIS is intended to enable the
combination of software components from multiple middleware 
vendors. 

This project contains appropriate files for this MCU family 
taken from CMSIS. A full copy of the CMSIS files, together
with additional information on CMSIS can be found at:

  http://www.arm.com/cmsis/

Documentation
~~~~~~~~~~~~~
The standard CMSIS documentation can be found within the
Code Red IDE help system, via:

Help -> Help Contents -> Cortex Microcontroller Software
                                         Interface Standard

More information on the use of CMSIS within the 
LPCXpresso IDE can be found in the LPCXpresso FAQ area of the
LPCware website at:

  http://www.lpcware.com/

At the time of writing, the CMSIS FAQ can be found directly
at:

  http://www.lpcware.com/content/faq/lpcxpresso/cmsis-support