LPC5410x FLASH read/write example
===========================================

Example description
-------------------
The IAP example demonstrates programming a FLASH block during run-time. For
this example, the code is running from FLASH and a FLASH block not used for
the executing code will be erased and programmed with some data. The example
also toggles the LED in the systick interrupt. The interrupts need to be
disabled during the IAP calls that change FLASH data and re-enabled after
the calls are complete.>br>

Do not run this example too many times or set it up to repeatedly erase and
reprogram FLASH as it will wear out FLASH.

Special connection requirements
-------------------------------
There are no special connection requirements for this example.

Build procedures:
-----------------
Visit the at 'LPCOpen quickstart guides' [http://www.lpcware.com/content/project/lpcopen-platform-nxp-lpc-microcontrollers/lpcopen-v200-quickstart-guides]
to get started building LPCOpen projects.