LPC5410x Repetitive Timer example
============================

Example description
-------------------
This example shows how to setup and use the repetitive timer to
generate a periodic timer tick interrupt. The timer is setup for
a set period and each interrupt will toggle the LED.

Special connection requirements
-------------------------------
There are no special connection requirements for this example.

Build procedures:
-----------------
Visit the at 'LPCOpen quickstart guides' [http://www.lpcware.com/content/project/lpcopen-platform-nxp-lpc-microcontrollers/lpcopen-v200-quickstart-guides]
to get started building LPCOpen projects.