LPC5410x I2C slave with DMA ROM API example
============================

Example description
-------------------
This example shows how to use the I2C slave ROM API to setup the I2C
slave bus for a transfer using DMA ROM API. Once the transfer starts,
the status of the transfer is polled for completion.

Special connection requirements
-------------------------------
To use this example, an I2C bus master must be connected to the I2C
slave signals. The master should use I2C address 0x18.

Build procedures:
-----------------
Visit the at 'LPCOpen quickstart guides' [http://www.lpcware.com/content/project/lpcopen-platform-nxp-lpc-microcontrollers/lpcopen-v200-quickstart-guides]
to get started building LPCOpen projects.