CLKOUT Example
==============

Example Description
-------------------
This example shows how to use the SYSCTL driver to enable a specific
clock source on the CLKOUT pin. To use this example, you'll need to
connect an oscilloscope to the CLKOUT pin on your board. See the
comments in the code for mapped pins for supported boards.

Using the standard configuration: standard clock initialization, using internal
clock only the demo will output the following:
	-- 24MHZ clock for 30-seconds
	-- 12MHz clock for 30-seconds
	-- 523kHz clock for 30-seconds
This sequence repeats indefinitely.

Special Connection Requirements
-------------------------------
Board [NXP_LPCXPRESSO_812]:
There are no special connection requirements for this example.

Board [NXP_812_MAX]:
There are no special connection requirements for this example.

Board [NXP_LPCXPRESSO_824]:
There are no special connection requirements for this example.
However, the easiest way to connect the clock is to flip the board over
and connect to P3-1 for ground; and P3-11, for the clock output.

Build procedures:
Visit the <a href="http://www.lpcware.com/content/project/lpcopen-platform-nxp-lpc-microcontrollers/lpcopen-v200-quickstart-guides">LPCOpen quickstart guides</a>
to get started building LPCOpen projects.