General Purpose Input/Output Example
====================================

Example Description
-------------------
The General Purpose Input/Output example demonstrates how to use the GPIO functions
for multiple GPIO pin functions at once. The example sets port 0 pins 0-3 (0-1 on 824)
to GPIO outputs.  It then demonstrates masked write operations on P0 using
an incrementing counter.  Output can be observed on port 0 pins 0-3 (0-1 on 824).

Special connection requirements
-------------------------------
Board [NXP_LPCXPRESSO_812]:
There are no special connection requirements for this example.

Board [NXP_812_MAX]:
There are no special connection requirements for this example.

Board [NXP_LPCXPRESSO_824]:
There are no special connection requirements for this example.

Build procedures:
Visit the <a href="http://www.lpcware.com/content/project/lpcopen-platform-nxp-lpc-microcontrollers/lpcopen-v200-quickstart-guides">LPCOpen quickstart guides</a>
to get started building LPCOpen projects.