SysTick Example
===============

Example Description
-------------------
The SysTick example simply blinks an LED at a periodic rate using the SysTick
interrupt. The LED is toggled in the SysTick interrupt handler.

Special Connection Requirements
-------------------------------
Board [NXP_LPCXPRESSO_812]:
There are no special connection requirements for this example.

Board [NXP_812_MAX]:
There are no special connection requirements for this example.

Board [NXP_LPCXPRESSO_824]:
There are no special connection requirements for this example.

Build procedures:
Visit the <a href="http://www.lpcware.com/content/project/lpcopen-platform-nxp-lpc-microcontrollers/lpcopen-v200-quickstart-guides">LPCOpen quickstart guides</a>
to get started building LPCOpen projects.