Overview
========
The Multicore Hello World demo application demonstrates how to set up projects for individual cores
on a multicore system. In this demo, the primary core releases the secondary core from the reset,
then prints the "Hello World from the Primary Core!" string to the terminal using the KSDK UART
drivers. The secondary core toggles an on-board LED indicating that the secondary core is running.
It is also possible to stop/start the secondary core during the runtime by pressing SW1/SW2 on-board buttons.
The on-board LED then indicates the change, it stops/starts toggling accordingly.

Toolchain supported
===================
- IAR embedded Workbench 7.80.4
- Keil MDK 5.21a
- MCUXpresso0.8

Hardware requirements
=====================
- Mini/micro USB cable
- LPCXpresso54114 board
- Personal Computer

Board settings
==============
No special settings are required.

Prepare the Demo
================
1.  Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J7) on the board
2.  Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board.
4.  Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo
================
The log below shows the output of the hello world multicore demo in the terminal window:
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
Starting Secondary core.

Hello World from the Primary Core!

Press the SW1 button to Stop Secondary core.
Press the SW2 button to Start Secondary core.
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
Customization options
=====================