![]() |
Linux NFC User Mode Stack
|
NFC NDEF Message information structure definition. More...
#include <linux_nfc_api.h>
Public Attributes | |
| int | is_ndef |
| The flags to indicate if it contains ndef record. More... | |
| unsigned int | current_ndef_length |
| Existing Ndef message length. More... | |
| unsigned int | max_ndef_length |
| Max Ndef message length can be written. More... | |
| int | is_writable |
| The flags to indicate if writing a Ndef message is supprted. More... | |
NFC NDEF Message information structure definition.
Definition at line 191 of file linux_nfc_api.h.
| unsigned int ndef_info_t::current_ndef_length |
Existing Ndef message length.
Definition at line 201 of file linux_nfc_api.h.
| int ndef_info_t::is_ndef |
The flags to indicate if it contains ndef record.
Definition at line 196 of file linux_nfc_api.h.
| int ndef_info_t::is_writable |
The flags to indicate if writing a Ndef message is supprted.
Definition at line 211 of file linux_nfc_api.h.
| unsigned int ndef_info_t::max_ndef_length |
Max Ndef message length can be written.
Definition at line 206 of file linux_nfc_api.h.
1.8.9.1