![]() |
Linux NFC User Mode Stack
|
NFC handover bluetooth record structure definition. More...
#include <linux_nfc_api.h>
Public Attributes | |
| nfc_handover_cps_t | power_state |
| Handover Carrier Power State. More... | |
| nfc_handover_bt_type_t | type |
| Handover bluetooth carrier configuration record type. More... | |
| unsigned char * | ndef |
| Handover Carrier Configuration record. More... | |
| unsigned int | ndef_length |
| Handover Carrier Configuration record length. More... | |
| unsigned char | address [6] |
| Bluetooth address. More... | |
| unsigned char * | device_name |
| Handover Carrier Data Reference name. More... | |
| unsigned int | device_name_length |
| Handover Carrier Data Reference name length. More... | |
NFC handover bluetooth record structure definition.
Definition at line 217 of file linux_nfc_api.h.
| unsigned char nfc_btoob_pairing_t::address[6] |
Bluetooth address.
Definition at line 238 of file linux_nfc_api.h.
| unsigned char* nfc_btoob_pairing_t::device_name |
Handover Carrier Data Reference name.
Definition at line 242 of file linux_nfc_api.h.
| unsigned int nfc_btoob_pairing_t::device_name_length |
Handover Carrier Data Reference name length.
Definition at line 246 of file linux_nfc_api.h.
| unsigned char* nfc_btoob_pairing_t::ndef |
Handover Carrier Configuration record.
Definition at line 230 of file linux_nfc_api.h.
| unsigned int nfc_btoob_pairing_t::ndef_length |
Handover Carrier Configuration record length.
Definition at line 234 of file linux_nfc_api.h.
| nfc_handover_cps_t nfc_btoob_pairing_t::power_state |
Handover Carrier Power State.
Definition at line 222 of file linux_nfc_api.h.
| nfc_handover_bt_type_t nfc_btoob_pairing_t::type |
Handover bluetooth carrier configuration record type.
Definition at line 226 of file linux_nfc_api.h.
1.8.9.1