![]() |
Linux NFC User Mode Stack
|
NFC handover select record structure definition. More...
#include <linux_nfc_api.h>
Public Attributes | |
| nfc_btoob_pairing_t | bluetooth |
| Bluetooth Handover select. More... | |
| nfc_wifi_pairing_t | wifi |
| Wifi Handover select. More... | |
NFC handover select record structure definition.
Definition at line 321 of file linux_nfc_api.h.
| nfc_btoob_pairing_t nfc_handover_select_t::bluetooth |
Bluetooth Handover select.
Definition at line 326 of file linux_nfc_api.h.
| nfc_wifi_pairing_t nfc_handover_select_t::wifi |
Wifi Handover select.
Definition at line 330 of file linux_nfc_api.h.
1.8.9.1