![]() |
Linux NFC User Mode Stack
|
NFC tag information structure definition. More...
#include <linux_nfc_api.h>
Public Attributes | |
| unsigned int | technology |
| indicates the technology of tag More... | |
| unsigned int | handle |
| the handle of tag More... | |
| char | uid [32] |
| the uid of tag More... | |
| unsigned int | uid_length |
| the uid length More... | |
| tNFC_PROTOCOL | protocol |
| activated protocol More... | |
NFC tag information structure definition.
Definition at line 164 of file linux_nfc_api.h.
| unsigned int nfc_tag_info_t::handle |
the handle of tag
Definition at line 173 of file linux_nfc_api.h.
| tNFC_PROTOCOL nfc_tag_info_t::protocol |
activated protocol
Definition at line 185 of file linux_nfc_api.h.
| unsigned int nfc_tag_info_t::technology |
indicates the technology of tag
Definition at line 169 of file linux_nfc_api.h.
| char nfc_tag_info_t::uid[32] |
the uid of tag
Definition at line 177 of file linux_nfc_api.h.
| unsigned int nfc_tag_info_t::uid_length |
the uid length
Definition at line 181 of file linux_nfc_api.h.
1.8.9.1