![]() |
Linux NFC User Mode Stack
|
NFC wifi handover select record structure definition. More...
#include <linux_nfc_api.h>
Public Attributes | |
| nfc_handover_cps_t | power_state |
| Handover Carrier Power State. More... | |
| unsigned char * | ndef |
| Handover Carrier Configuration record. More... | |
| unsigned int | ndef_length |
| Handover Carrier Configuration record length. More... | |
| unsigned char * | ssid |
| Wifi network ssid. More... | |
| unsigned int | ssid_length |
| Wifi network ssid length. More... | |
| unsigned char * | key |
| Wifi netwrok key. More... | |
| unsigned int | key_length |
| Wifi netwrok key length. More... | |
NFC wifi handover select record structure definition.
Definition at line 252 of file linux_nfc_api.h.
| unsigned char* nfc_wifi_pairing_t::key |
Wifi netwrok key.
Definition at line 277 of file linux_nfc_api.h.
| unsigned int nfc_wifi_pairing_t::key_length |
Wifi netwrok key length.
Definition at line 281 of file linux_nfc_api.h.
| unsigned char* nfc_wifi_pairing_t::ndef |
Handover Carrier Configuration record.
Definition at line 261 of file linux_nfc_api.h.
| unsigned int nfc_wifi_pairing_t::ndef_length |
Handover Carrier Configuration record length.
Definition at line 265 of file linux_nfc_api.h.
| nfc_handover_cps_t nfc_wifi_pairing_t::power_state |
Handover Carrier Power State.
Definition at line 257 of file linux_nfc_api.h.
| unsigned char* nfc_wifi_pairing_t::ssid |
Wifi network ssid.
Definition at line 269 of file linux_nfc_api.h.
| unsigned int nfc_wifi_pairing_t::ssid_length |
Wifi network ssid length.
Definition at line 273 of file linux_nfc_api.h.
1.8.9.1