![]() |
Linux NFC User Mode Stack
|
NFC SNEP server callback function structure definition. More...
#include <linux_nfc_api.h>
Public Attributes | |
| void(* | onDeviceArrival )() |
| NFC Peer Device callback function when device is detected. More... | |
| void(* | onDeviceDeparture )(void) |
| NFC Peer Device callback function when device is removed. More... | |
| void(* | onMessageReceived )(unsigned char *message, unsigned int length) |
| NFC Peer Device callback function when NDEF message is received from peer device. More... | |
NFC SNEP server callback function structure definition.
Definition at line 352 of file linux_nfc_api.h.
| void(* nfcSnepServerCallback_t::onDeviceArrival) () |
NFC Peer Device callback function when device is detected.
Definition at line 356 of file linux_nfc_api.h.
| void(* nfcSnepServerCallback_t::onDeviceDeparture) (void) |
NFC Peer Device callback function when device is removed.
Definition at line 361 of file linux_nfc_api.h.
| void(* nfcSnepServerCallback_t::onMessageReceived) (unsigned char *message, unsigned int length) |
NFC Peer Device callback function when NDEF message is received from peer device.
| message | NDEF message |
| length | NDEF message length |
Definition at line 368 of file linux_nfc_api.h.
1.8.9.1