WELCOME to the MPC555 Start-up Pack

This is the README.TXT file for the m555r223.zip file. This file has everything
you need to start writing C programs for the mpc555 except the compiler. It
defines all of the registers and bit fields for them MPC555.

The last big changes were release 2.20 with updates to the register names to make
them match the March 1, 1999 release of the MPC555 User's Manual. The only major
change was the addition of 32 bit access to TPU parameter RAM. To accomodate this
change accessing the TPU parameters was changed:

old style:
TPU_A.PARM[channel][param].R == 1;

new style:
TPU_A.PARM.R[channel][param] == 1;

To access the TPU parameter RAM using 32 bit is done as shown:

TPU_A_PARAM.L[channel][param] == 0x12345678;

32 bit parameters are number 0-3.

A complete history of the changes to the MPC555 start-up pack is listed in the
file HISTORY.TXT. Starting with release 2.00 the header file is seperated by 
modules. This means that only the modules needed are included in a file, this 
greatly reduces compile time.

The mpc555 registers can be used three different ways. There is an example
program to show each of the different ways (example1.c, example2.c and
example3.c). Each way to use the header file has advantages and disadvantages:

example1.c  (fixed strucutre)
-----------------------------
Advantage:    Easy to use, just include mpc555.h file.
Disadvantage: Generates larger slower code.
              Takes longer to compile.

exmaple2.c  (Diab sections)
---------------------------
Advantage:    Generates smaller faster code.
              Faster to compile.
Disadvantage: Harder to use.
              Only works with Diab compiler.

example3.c  (global pointers)
-----------------------------
Advantage:    Generates smaller faster code.
              Faster to compile.
Disadvantage: Harder to use.
              Uses 15 global pointers.

When using Diab sections or global pointers you must #define Main_Program in 
your main program only and #include "mpc555.h". You must define Main_Program 
before you include mpc555.h. When using Diab sections or global pointers you 
only need to include the modules that a file uses, see mpc555.c for an example.

When using Diab sections or global pointers you must also define DIAB_SECTIONS
or HEADER_POINTERS when compiling every file. You can do this by uncommenting
the defines in the m_common.h file or by adding the define to the makefile 
(look at the included makefile for an example).

This start-up pack has been setup using the Diab Data compiler, changes may
be needed for other compilers. This zip file contains the following files:

mpc555.h    -The header file for the MPC555 it defines all of the mpc555
             registers and bit fields in the registers.

m_common.h  -Common type definitions and configuration.

m_flash.h   -Header file for the CMF FLASH modules.

m_qadc.h    -Header file for the QADC modules.

m_qsmcm.h   -Header file for the QSMCM module.

m_mios1.h   -Header file for the MIOS1 module.

m_toucan.h  -Header file for the TOUCAN modules.

m_tpu3.h    -Header file for the TPU3 modules.

m_sram.h    -Header file for the SRAM modules.

m_dptram.h  -Header file for the DPTRAM module.

m_uimb.h    -Header file for the UIMB module.

m_usiu.h    -Header file for the USIU module.

mpc555.c    -This file contains general setup code for using the mpc555.

example1.c  -This a a simple program that shows how to use the standard 
             set-up files and headers using the fixed structure method.

example2.c  -This a a simple program that shows how to use the standard 
             set-up files and headers using the diab sections method.

example3.c  -This a a simple program that shows how to use the standard 
             set-up files and headers using the global pointers method.

makefile    -A makefile to build the three example programs. It requires a 
             make program.

ex_tbl.s   -This file contains the exception table definitions for MPC500
            devices. All exception routines are extern and imported to 
            this file.        

ex_tblc.s  -This file contains the reduced size exception table definitions
            for the MPC555 using the exception table relocation feature.
            All exception routines are extern and imported to this file.

ex_funcs.c -This file contains empty exception routines that are referenced 
            by the exception table file ex_tbl.s or ex_tblc.s. (This file
            mat need to be changed for a different compiler)

mpc555.dld  -This is a linker file for the mpc555. (This is specific
             to the Diab linker). 

crt0etas.s  -This is the file that configures the system and them calls the C
             main function. This is the standard file from Diab with a call to
             the mpc555 setup routine inserted. (This file will be different 
             for every compiler)

etas555.wsp -A SDS debugger workspace file for the ETAS 555 EVB. A couple
             changes were made to the file that comes with the SDS debugger,
             you will need to use this file if you are using the ETAS555 EVB.

history.txt -A history of changes to the mpc555 start-up pack.

If you do not have a make program, try using GNU make. You can get GNU
make for windows at http://sourceware.cygnus.com/cygwin/ and for DOS at
http://www.delorie.com/djgpp/.

If you have any questions please feel free to contact me or send an email
to the MPC500 mailing list at mpc500@oakhill-csic.sps.mot.com.

-Jeff
 29 Feb. 2000
__________________________________________________________________
\ Jeff Loeliger                      Motorola SPS                 \
 \ mailto:r12110@email.sps.mot.com   Systems Engineering Department\
  \ phone: +44-1355-35-5400          Powertrain Systems Division    \
   \ fax : +44-1355-35-6300          East Kilbride, Scotland         \
    \ Motorola Internal: http://ncsg-euroweb.sps.mot.com/~r12110      \
     \_________________________________________________________________\