NXP® SemiconductorsMSE9S12UF32_1L47S
Mask Set ErrataRev. April 17, 2012



MC9S12UF32, Mask 1L47S


Introduction
This errata sheet applies to the following devices:

MC9S12UF32



MCU Device Mask Set Identification

The mask set is identified by a 5-character code consisting of a version number, a letter, two numerical digits, and a letter, for example 1K79X. All standard devices are marked with a mask set number and a date code.



MCU Device Date Codes

Device markings indicate the week of manufacture and the mask set used. The date is coded as four numerical digits where the first two digits indicate the year and the last two digits indicate the work week. For instance, the date code "0201" indicates the first week of the year 2002.



MCU Device Part Number Prefixes

Some MCU samples and devices are marked with an SC, PC, or XC prefix. An SC prefix denotes special/custom device. A PC prefix indicates a prototype device which has undergone basic testing only. An XC prefix denotes that the device is tested but is not fully characterized or qualified over the full range of normal manufacturing process variations. After full characterization and qualification, devices will be marked with the MC or SC prefix.



Errata System Tracking Numbers

MUCtsXXXXX is the tracking number for device errata. It can be used with the mask set and date code to identify a specific erratum.



Errata Summary


Errata NumberModule affectedBrief DescriptionWork-
around
MUCts01498 ique Security cannot be disabled via BDM unsecure command sequence YES
MUCts01659 ata5hc Invalid UDMA write sequence in a corner case YES
MUCts01665 ique Reset sequence in double buffer mode YES
MUCts01861 S12_bdm Possible manipulation of return address when exiting BDM active mode YES
MUCts02415 S12_mebi MEBI: Missing ECLK edge on first external access after mode switching YES
MUCts03031 tim_16b8c TIM:Normal Output Compare event happens on setting OC7M bit if OM/OL=0 YES
MUCts04160 tim_16b8c TIM_16B8C: Output compare pulse is inaccurate YES
MUCts04246 sci SCI: RXEDGIF occurs more times than expected in IR mode YES



Security cannot be disabled via BDM unsecure command sequenceMUCts01498

Description

When security is enabled (MCU is reset with bits[1:0] of the flash 

security byte at address $FF0F set to '00', '01' or '11'), security
cannot be disabled using the BDM mass erase/security byte reprogram
sequence. A bug causes the blank check (performed by the BDM secure
firmware) to fail and as a result the flash security byte cannot be
reprogrammed to the unsecure state.

Workaround


Do not enable security by leaving bits[1:0] of the flash security byte 

programmed to '10'. (Ensure that these bits are programmed to '10'
BEFORE resetting the MCU otherwise security will be enabled).

OR

The security can be disabled by reprogramming bits[1:0] of the security
byte to '10' using a software routine embedded within the user program.
The routine could, for example, be initiated by a user specified
command issued through the SCI interface.





Invalid UDMA write sequence in a corner caseMUCts01659

Description

An invalid UDMA write sequence exists under a specific condition:

1) IQUE buffer is empty
2) ATA5HC controller buffer is not full
3) ATA device issues a transfer pausing with a termination sequence
4) USB receiver has just received a packet and stored it in the IQUE
buffer
If all of the above conditions occur simultaneously, this will result in
a word being missed and the transfer hanging.

Workaround


Monitor the IQUE buffer in software and swap buffer resources out if 

~30
entries remain.





Reset sequence in double buffer modeMUCts01665

Description

The default reset state for the read/write enable signal of the FSM

Double Buffer Control circuit is low which allows read/write operations
during reset. This will result in a cycle of false read/write
acknowledge signals following reset if the Transmit Request or Receive
Request signals are asserted.

Workaround


Change the QCnREQ value to $FF before resetting the IQUE module or

Double Buffer Controller.



Possible manipulation of return address when exiting BDM active modeMUCts01861

Description

Upon leaving BDM active mode, the CPU return address is stored

temporarily for a few cycles in the BDM shift register. If a BDM command
transmission is detected during this time, the return address will be
manipulated in the BDM shift register. This situation is likely to occur
when a CPU BGND instruction is executed in user code during debugging
under the following conditions:

(i) The BDM module is not enabled AND
(ii) BDM commands are sent from the host

If this situation occurs, the CPU will execute BDM firmware and will
check the status of the ENBDM bit in the BDMSTS register. If the BDM is
disabled, the ENBDM bit will be clear, and hence the BDM firmware will
be exited and the shift register manipulation described above will occur.

Workaround


Avoid using the BGND instruction when the ENBDM bit in the BDMSTS

register is cleared.



MEBI: Missing ECLK edge on first external access after mode switchingMUCts02415

Description

If the ECLK is used as an external bus control signal (ESTR=1) the first

external access is lost after switching from a single chip mode with
enabled ECLK output to an expanded mode. The ECLK is erroneously held in
the high phase thus the first external bus access does not generate a
rising ECLK edge for the external logic to latch the address. The ECLK
stretches low after the lost access resulting in all following external
accesses to be valid.

Workaround


Enter expanded mode with ECLK output disabled (NECLK=1). Enable the ECLK

after switching the mode before executing the first external access.



TIM:Normal Output Compare event happens on setting OC7M bit if OM/OL=0 MUCts03031

Description

When an OC7M bit is set, an erroneous normal output compare event can 

happen on a timer port if the compare action is selected as "Timer
disconnected from output pin logic ".

Corresponding configuration:
* TIOSx = 1 --> Output compare mode
* OMx = OLx = 0 --> Output compare logic disconnected from the pin
* OC7Mx = 1 --> Mask bit set for OC7 event







Workaround


Set OC7Mx = 1 only for channels where the output compare action should 

drive the pin, and OC7Mx = 0 for all other channels where the pin is
required to be disconnected from the output compare logic.



TIM_16B8C: Output compare pulse is inaccurateMUCts04160

Description

The pulse width of an output compare (which resets the free running

counter when TCRE = 1) will measure one more bus clock cycle than
expected.



Workaround


The specification has been updated. Please refer to revision 01.05 (05 

May 2010) or later.

In description of bitfield TCRE in register TSCR2,a note has been added:
TCRE=1 and TC7!=0, the TCNT cycle period will be TC7 x "prescaler
counter width" + "1 Bus Clock". When TCRE is set and TC7 is not equal to
0, then TCNT will cycle from 0 to TC7. When TCNT reaches TC7 value, it
will last only one bus cycle then reset to 0.








SCI: RXEDGIF occurs more times than expected in IR modeMUCts04246

Description

Configured for Infrared Receive mode, the SCI may incorrectly set the 

RXEDGIF bit if there are consecutive '00' data bits. There are two
cases:

Case 1: due to re-sync of the RXD input, the received edge may be
delayed by one bus cycle. If an edge (bit = '0') is detected near
an SCI clock edge, the next edge (bit = '0') may be detected one
SCI clock later than expected due to re-sync logic.

Case 2: if external baud is slower than SCI receiver, the next edge
may be detected later than expected.

This glitch can be detected by the RXEDGIF circuit, but it does not
impact the final data result because the SCI receive and data recovery
logic takes samples at RT8, RT9, and RT10.




Workaround


Case 1 and case 2 may occurs at same time. To avoid those unexpected 

RXEDGIF at IR mode, the external baud should be kept a little bit
faster than receiver baud by:
P > (1/16)/(SBR)
or
(P)(SBR)(16)> 1

Where SBR is baud of receiver, P is external baud faster ratio.
For example:
1.- When SBR = 16, P = 0.4%, this means the external baud should be at
least 0.4% faster than receiver.
2.- When SBR = 4, P = 1.6%, this means the external baud should be at
least 1.6% faster than receiver.

Case 1 will cover case 2, i.e. case 1 is the worst case. If case1 is
solved, case 2 is also solved.


© NXP Semiconductors, Inc., 2012. All rights reserved.