![]() |
ISF
2.1
Intelligent Sensing Framework for Kinetis with Processor Expert
|
#include "ISFCore1.h"
Go to the source code of this file.
Functions | |
| ci_response_enum | rli_ci_app_callback (ci_host_cmd_packet_t *, ci_app_resp_packet_t *) |
| ci_response_enum | App1_ci_app_callback (ci_host_cmd_packet_t *, ci_app_resp_packet_t *) |
| void | PM_task (uint32_t task_init_data) |
| void | CI_task (uint32_t task_init_data) |
Variables | |
| const ci_funcp_t | ci_callback [] |
| Command interpreter callbacks. The array index is the application ID. More... | |
Definition in file ISFCore1.c.