![]() |
ISF
2.1
Intelligent Sensing Framework for Kinetis with Processor Expert
|

Go to the source code of this file.
Variables | |
| mpl3115_Sensor_Specific_Settings_t | MPL3115_1_Sensor_Specific_Config |
| This allows access to the sensor specific configuration for the target sensor. More... | |
| const isf_dsa_Adapter_t | MPL3115_1_Adapter |
| This creates the sensor adapter instance for the target sensor. More... | |
| const i2c_device_t | MPL3115_1_DeviceInfo |
| This allows access to the sensor communications specific configuration. More... | |
Definition in file MPL3115_1.c.