![]() |
ISF
2.1
Intelligent Sensing Framework for Kinetis with Processor Expert
|

Go to the source code of this file.
Functions | |
| void | Fusion_Task_task (uint32_t task_init_data) |
| void | MagCal_Task_task (uint32_t task_init_data) |
Variables | |
| fsl_fusion_Sensor_Specific_Settings_t | ORIENT_1_Sensor_Specific_Config |
| This allows access to the sensor specific configuration for the target sensor. More... | |
| const isf_dsa_Adapter_t | ORIENT_1_Adapter |
| This creates the sensor adapter instance for the target sensor. More... | |
Definition in file ORIENT_1.c.