![]() |
ISF
2.1
Intelligent Sensing Framework for Kinetis with Processor Expert
|
#include "PE_Types.h"#include "PE_Error.h"#include "PE_Const.h"#include "IO_Map.h"#include "Cpu.h"#include "isf.h"#include "isf_ci_protocol.h"

Go to the source code of this file.
Macros | |
| #define | __CDEUserType_Protocol1_Type |
Typedefs | |
| typedef int32_t | Protocol1_Type |
Functions | |
| int32_t | Protocol1_ProtocolCallBack (uint32_t anumBytes, uint8_t *apSrc, uint32_t *apnumDestBytes, uint8_t *apDest) |
| int32_t | Protocol1_ProtocolInit (int8_t aprotocolID, void *apInitData) |
Definition in file Protocol1.h.