![]() |
ISF
2.1
Intelligent Sensing Framework for Kinetis with Processor Expert
|
This component "Serial_LDD" implements an asynchronous serial communication. The component supports different settings of parity, word width, stop-bit and communication speed, user can select interrupt or polling handler. Communication speed can be changed also in runtime. The component requires one on-chip asynchronous serial communication channel. More...
#include "Cpu.h"

Go to the source code of this file.
Data Structures | |
| struct | Serial_ISF_UART1_TDeviceData |
Macros | |
| #define | Serial_ISF_UART1_PRPH_BASE_ADDRESS 0x4006A000U |
| #define | Serial_ISF_UART1_Init_METHOD_ENABLED |
| #define | Serial_ISF_UART1_SendBlock_METHOD_ENABLED |
| #define | Serial_ISF_UART1_ReceiveBlock_METHOD_ENABLED |
| #define | Serial_ISF_UART1_OnBlockReceived_EVENT_ENABLED |
| #define | Serial_ISF_UART1_OnBlockSent_EVENT_ENABLED |
| #define | ENABLED_TX_INT 0x01U |
| #define | BREAK_DETECTED 0x02U |
| #define | TX_COMPLETED 0x04U |
| #define | ENABLE_TX_COMPLETE 0x10U |
Typedefs | |
| typedef Serial_ISF_UART1_TDeviceData * | Serial_ISF_UART1_TDeviceDataPtr |
Functions | |
| LDD_TDeviceData * | Serial_ISF_UART1_Init (LDD_TUserData *UserDataPtr) |
| Initializes the device. Allocates memory for the device data structure, allocates interrupt vectors and sets interrupt priority, sets pin routing, sets timing, etc. If the "Enable
in init. code" is set to "yes" value then the device is also enabled(see the description of the Enable() method). In this case the Enable() method is not necessary and needn't to be generated. More... | |
| LDD_TError | Serial_ISF_UART1_ReceiveBlock (LDD_TDeviceData *DeviceDataPtr, LDD_TData *BufferPtr, uint16_t Size) |
| Specifies the number of data to receive. The method returns ERR_BUSY until the specified number of characters is received. Method [CancelBlockReception] can be used to cancel a running receive operation. If a receive operation is not in progress (the method was not called or a previous operation has already finished) all received characters will be lost without any notification. To prevent the loss of data call the method immediately after the last receive operation has finished (e.g. from the [OnBlockReceived] event). This method finishes immediately after calling it - it doesn't wait the end of data reception. Use event [OnBlockReceived] to check the end of data reception. More... | |
| LDD_TError | Serial_ISF_UART1_SendBlock (LDD_TDeviceData *DeviceDataPtr, LDD_TData *BufferPtr, uint16_t Size) |
| Sends a block of characters. The method returns ERR_BUSY when the previous block transmission is not completed. Method [CancelBlockTransmission] can be used to cancel a transmit operation. This method is available only if the transmitter property is enabled. This method finishes immediately after calling it - it doesn't wait the end of data transmission. Use event [OnBlockSent] to check the end of data transmission. More... | |
| void | Serial_ISF_UART1_Interrupt (LDD_RTOS_TISRParameter _isrParameter) |
This component "Serial_LDD" implements an asynchronous serial communication. The component supports different settings of parity, word width, stop-bit and communication speed, user can select interrupt or polling handler. Communication speed can be changed also in runtime. The component requires one on-chip asynchronous serial communication channel.
Definition in file Serial_ISF_UART1.h.