![]() |
ISF
2.1
Intelligent Sensing Framework for Kinetis with Processor Expert
|
| CAccelSensor | |
| CApp1AppInstance_t | |
| CApp1AppSettings_t | |
| CApp1SensorData_t | |
| Cbm_cb_config_t | |
| Cbm_t | |
| CBMTimer1_TDeviceData | |
| CbusHandle_struct | This structure is a declaration of a BusHandle type |
| Cci_app_resp_packet_t | This structure enables an application to read from or write to the host |
| Cci_ctrl_reg_t | Command Interpreter Control Register Structure. |
| Cci_host_cmd_packet_t | This structure contains host command information |
| Cci_protocol_t | This structure binds a protocol ID to a set of related functions and data. When a packet is received from the host, the CI task will invoke the callback that is associated with the protocol ID that is part of the CI packet header |
| Cci_regs_t | Command Interpreter Registers Structure. Contains all CI registers. |
| Cci_rx_packet_t | This structure holds information to receive a packet of data to the host. CI will fill the structure with the information as it receives it from the ISR and will notify the CI task when a packet has been fully received |
| Cci_stream_ctrl_reg1_t | Stream protocol control register 1 Structure |
| Cci_stream_instance_t | Stream instance structure is used internally to encapsulate the information of a stream and the current trigger state of the dataset(s) belonging to that stream. It also contains a pointer to the next stream to create a single linked list of streams |
| Cci_stream_regs_t | Stream protocol registers Structure. Contains stream protocol control registers |
| Cci_tx_packet_t | This structure holds information to send a packet of data to the host. A task will fill the structure with the information and enable transmit buffer empty. The ISR will send the data byte by byte until all data is sent |
| CconversionBuffer_t | |
| CdataPair_t | |
| Cdevice_cmd_packet_t | Rli overall application state buffer format |
| Cdevice_info_t | This structure holds the ROM device information such as version and part number and is returned by the _fw_device_info_get() command |
| CDeviceDescriptor_struct | Define the sensor device descriptor |
| Cdm_ChannelDescriptor_struct | This structure is a declaration of a channel descriptor type |
| Cdm_DeviceDescriptor_struct | This structure defines a handle for the device |
| CfLfiTable_t | |
| Cfquaternion | |
| Cfsl_fusion_DeviceDescriptor_t | |
| Cfsl_fusion_Sensor_Specific_Settings_t | |
| Cfsl_orientation_DataBuffer_t | |
| Cfusion_algorithmConfig_t | |
| Cfusion_state_t | |
| Cfxas21000_ODR_Table_tag | Structure defines the ODR table between Hybrid and normal mode of FXAS21000 operation |
| Cfxas21002_ConfigTable_tag | Structure defines the configuration table |
| Cfxas21002_DataBuffer_t | This structure defines the dummy DSA data buffer format |
| Cfxas21002_ODR_Table_tag | Structure defines the ODR table between Hybrid and normal mode of FXAS21002 operation |
| Cfxas21002_Sensor_Specific_Reg_t | |
| Cfxas21002_Sensor_Specific_Settings_t | |
| Cfxls8471_DataBuffer_t | This structure defines the dummy DSA data buffer format |
| Cfxls8471_Sensor_Specific_Reg_t | |
| Cfxls8471_Sensor_Specific_Settings_t | |
| Cfxls8471_Specific_Settings_t | This structure defines important settings |
| Cfxos8700_ConfigTable_tag | Structure defines the configuration table |
| Cfxos8700_DataBuffer_t | This structure defines the dummy DSA data buffer format |
| Cfxos8700_ODR_Table_tag | Structure defines the ODR table between Hybrid and normal mode of device operation |
| Cfxos8700_Sensor_Specific_Reg_t | |
| Cfxos8700_Sensor_Specific_Settings_t | |
| Cgyro_config_t | The structure defines the FXAS21002 configuration |
| CGyroSensor | |
| Ci2c_deviceEndpoint_struct | This structure defines a device endpoint encapsulation for i2c handler |
| Ci2c_instance_PEx | This structure contains i2c LLD function pointers |
| Ci2c_Master_BusConfig_struct | |
| Ci2c_Master_BusHandle_struct | This structure defines the data bus handle |
| CI2CDeviceInfo | Information necessary to communicate with an I2C slave device |
| CI2CMasterState | Internal driver state information |
| Cisf_Acceleration1D_EngFixed_t | Standard fixed type for single axis accelerometers |
| Cisf_Acceleration1D_Float_t | Standard float type for single axis accelerometers |
| Cisf_Acceleration2D_EngFixed_t | Standard fixed type for two axis accelerometers |
| Cisf_Acceleration2D_Float_t | Standard float type for two axis accelerometers |
| Cisf_Acceleration3D_EngFixed_t | Standard fixed type for three axis accelerometers |
| Cisf_Acceleration3D_Float_t | Standard float type for three axis accelerometers |
| Cisf_AngularVelocity1D__float_t | Standard fixed type for single axis accelerometers |
| Cisf_AngularVelocity1D_EngFixed_t | Standard fixed type for single axis accelerometers |
| Cisf_AngularVelocity2D__float_t | Standard fixed type for two axis accelerometers |
| Cisf_AngularVelocity2D_EngFixed_t | Standard fixed type for two axis accelerometers |
| Cisf_AngularVelocity3D__float_t | Standard fixed type for three axis accelerometers |
| Cisf_AngularVelocity3D_EngFixed_t | Standard fixed type for three axis accelerometers |
| Cisf_DegreesCelsius1D_EngFixed_t | Standard fixed type for single axis pressure sensor |
| Cisf_DegreesCelsius1D_float_t | Standard floating point type for single axis temperature sensor |
| Cisf_dsa_Adapter_st | This defines the DSA adapter structure required for static initialization of the concrete instance of a given sensor adapter |
| Cisf_dsa_ControlData_st | This defines the DSA adapter functional interface |
| Cisf_dsa_ControlInterface_st | This defines the DSA adapter control interface abstract function list |
| Cisf_dsa_DeviceInfoBlock_st | This defines the DSA adapter device information block |
| Cisf_dsa_info_t | |
| Cisf_dsa_SensorSettings_st | This defines the DSA sensor configuration parameter structure configuring the sensor settings by a subscriber task |
| Cisf_fifo_t | |
| Cisf_KiloPascals1D_EngFixed_t | Standard fixed type for single axis pressure sensor |
| Cisf_KiloPascals1D_float_t | Standard floating point type for single axis pressure sensor |
| Cisf_lib_info_t | This structure holds the ISF library information such as version and part number |
| Cisf_MagneticFieldStrength1D_EngFixed_t | Isf_SensorDataTypes_t TYPE_MAGNETIC_FIELD_STRENGTH_1D |
| Cisf_MagneticFieldStrength1D_float_t | Standard fixed type for single axis accelerometers |
| Cisf_MagneticFieldStrength2D_EngFixed_t | Isf_SensorDataTypes_t TYPE_MAGNETIC_FIELD_STRENGTH_2D |
| Cisf_MagneticFieldStrength2D_float_t | Standard fixed type for two axis accelerometers |
| Cisf_MagneticFieldStrength3D_EngFixed_t | Isf_SensorDataTypes_t TYPE_MAGNETIC_FIELD_STRENGTH_3D |
| Cisf_MagneticFieldStrength3D_float_t | Standard fixed type for three axis accelerometers |
| Cisf_Meters1D_EngFixed_t | Standard fixed type for single axis altitude sensor |
| Cisf_Meters1D_float_t | Standard floating point type for single axis altitude sensor |
| Cisf_Orientation3D_Euler_EngFloat_t | |
| Cisf_Orientation3D_Quaterion_EngFloat_t | |
| Cisf_Orientation3D_Rotation_EngFloat_t | |
| Cisf_SensorHandle_st | This defines the DSA sensor device handle structure used to invoke the adapter access functions |
| Cisf_SubscriptionSettings_t | |
| Cmag3110_DataBuffer_t | This structure defines the dummy DSA data buffer format |
| Cmag3110_Sensor_Specific_Reg_t | |
| Cmag3110_Sensor_Specific_Settings_t | |
| Cmag_config_t | The structure defines the MAG3110 configuration |
| CMagCalibration | |
| CMagneticBuffer | |
| CMagSensor | |
| Cmma865x_DataBuffer_t | This structure defines the dummy DSA data buffer format |
| Cmma865x_Sensor_Specific_Reg_t | |
| Cmma865x_Sensor_Specific_Settings_t | |
| Cmma865x_Specific_Settings_t | This structure defines important settings |
| Cmpl3115_DataBuffer_t | This structure defines the dummy DSA data buffer format |
| Cmpl3115_Sensor_Specific_Reg_t | |
| Cmpl3115_Sensor_Specific_Settings_t | |
| Cmpl3115_Specific_Settings_t | This structure defines important settings |
| CPitUserConfig | PIT timer configuration structure |
| CPressureSensor | |
| Cprotocol_t | This structure contains protocol-specific function pointers and properties |
| Cqr_config_t | This structure holds the quick read configuration for all applicable mailboxes. The first 4 mailboxes are used for the command packet read/write. All other mailboxes can be configured as quick read |
| CrliAppState_t | |
| CrliAppStatus_t | Rli application configuration buffer format |
| CrliConfigRegister_t | |
| CSensorConfig_st | This defines the DSA sensor configuration structure defining each individual sensor adapter in the DSA Sensor List |
| CSensorInfo_t | |
| CsensorSampleData | |
| CSerial_ISF_UART1_TDeviceData | |
| Cspi_master_BusConfig_struct | |
| Cspi_master_CommSpecificInfo_t | |
| Cspi_master_Endpoint_struct | This structure defines a device endpoint encapsulation for spi handler |
| Cspi_master_instance_PEx | This structure contains i2c LLD function pointers |
| CSPI_Master_State | |
| Cspi_mater_BusHandle_struct | This structure defines the data bus handle |
| Cspi_mater_SlaveCmd | This structure defines the spi slave command format |
| Cspi_mater_slaveInfo | This structure defines the slave specific spi information |
| CSpiConfig | SPI hardware configuration settings |
| CSPIHandle | |
| CSPIUserConfig | Information about a device on the SPI bus |
| CSV_1DOF_P_BASIC | |
| CSV_3DOF_B_BASIC | |
| CSV_3DOF_G_BASIC | |
| CSV_3DOF_Y_BASIC | |
| CSV_6DOF_GB_BASIC | |
| CSV_6DOF_GY_KALMAN | |
| CSV_9DOF_GBY_KALMAN | |
| Csync_object_t | Type for an synchronization object |
| Csys_channelDescriptor_t | This structure defines the channel descriptor |
| CTU_instance_PEx_t | This structure contains Timer Unit LLD function pointers |
| Cuart_BusConfig_struct | |
| Cuart_BusHandle_struct | This structure defines the data bus handle |
| Cuart_deviceEndpoint_struct | This structure defines a device endpoint encapsulation for uart handler |
| Cuart_instance_PEx | This structure contains i2c LLD function pointers |
| CUartConfig | UART configuration structure |
| CUartState | Runtime state of the UART driver |
| CUartUserConfig | User configuration structure for UART driver |